<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 the internal pull resistor is automatically disabled</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/the-internal-pull-resistor-is-automatically-disabled/m-p/909354#M53311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking at the KM series' reference manual.&lt;BR /&gt;The following explanation is given in "11.6.1 Pin control".&lt;BR /&gt;"Note that the internal pull resistor is automatically disabled whenever the output buffer is enabled for the Pull Enable bit to remain set."&lt;/P&gt;&lt;P&gt;(1) Does the GPIO output port indicate that the built-in pull resistance can not be set or used?&lt;BR /&gt;(2) Is it pull enable, but is the output port pull resistance not allowed?&lt;BR /&gt;(3) In which case should you use the above? (The register is a pull permission, but there is no pull resistance.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you will.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jun 2019 03:01:02 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2019-06-12T03:01:02Z</dc:date>
    <item>
      <title>the internal pull resistor is automatically disabled</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/the-internal-pull-resistor-is-automatically-disabled/m-p/909354#M53311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking at the KM series' reference manual.&lt;BR /&gt;The following explanation is given in "11.6.1 Pin control".&lt;BR /&gt;"Note that the internal pull resistor is automatically disabled whenever the output buffer is enabled for the Pull Enable bit to remain set."&lt;/P&gt;&lt;P&gt;(1) Does the GPIO output port indicate that the built-in pull resistance can not be set or used?&lt;BR /&gt;(2) Is it pull enable, but is the output port pull resistance not allowed?&lt;BR /&gt;(3) In which case should you use the above? (The register is a pull permission, but there is no pull resistance.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you will.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 03:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/the-internal-pull-resistor-is-automatically-disabled/m-p/909354#M53311</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-06-12T03:01:02Z</dc:date>
    </item>
    <item>
      <title>Re: the internal pull resistor is automatically disabled</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/the-internal-pull-resistor-is-automatically-disabled/m-p/909355#M53312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;1. Yes, when the pin work as GPIO output, pull resistor is disabled.&lt;/P&gt;&lt;P&gt;2.Yes, it's sure that the pull resistor has no influence on output. And the Pull Enable bit in PCR register will not change.&lt;/P&gt;&lt;P&gt;3. When pin in output status. The functions apply across all digital pin muxing modes and individual peripherals do not&lt;BR /&gt;override the configuration in the Pin Control register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jun 2019 09:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/the-internal-pull-resistor-is-automatically-disabled/m-p/909355#M53312</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-06-12T09:35:55Z</dc:date>
    </item>
  </channel>
</rss>