<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K60F+USB Stack</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234223#M5328</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, thank you for the answer, I'm already using the usb stack examples of HID app, and it works but only with the twr-ser, but with the Twr-ser2, i cant get that the computer renognize ths usb device, I change the code to hability the high speed and do the jumper configuration, but still no luck. Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Apr 2013 13:53:44 GMT</pubDate>
    <dc:creator>xavi2804</dc:creator>
    <dc:date>2013-04-10T13:53:44Z</dc:date>
    <item>
      <title>TWR-K60F+USB Stack</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234221#M5326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am new here, I want to use the usb stack to create an usb 2.0 HID app with a TWR-K60F120M and TWR-SER2, but i dowload the usb_stack_v4.0.3 and in the realease notes it says that this board is not compatible, but the tower has the usb high speed controller, so how can i make this without the usb stack?. Also if i can use the usb stack is there any examples for this board, because i found for K70F and K60N. Thank you&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 17:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234221#M5326</guid>
      <dc:creator>xavi2804</dc:creator>
      <dc:date>2013-03-21T17:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F+USB Stack</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234222#M5327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; &lt;SPAN lang="ES-MX" style="font-family: 'Calibri','sans-serif'; font-size: 11pt; mso-fareast-font-family: Batang; mso-bidi-font-family: 'Times New Roman'; mso-ansi-language: ES-MX; mso-fareast-language: EN-US; mso-bidi-language: AR-SA;"&gt;Hello Javier,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As the Kinetis K60F120 and K70F120 devices shares the modules version, and TWR-K60F120M and TWR-K70FN1M has the same crystal value (50 MHz) and USB connections, you could load the provided examples for K70F120, into the K60F120, and they should work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additionally, you could also use Freescale MQX v4.0, which includes a BSP for TWR-K60F120M board and USB HID Device examples. This could be downloaded from &lt;A href="http://www.freescale.com/mqx"&gt;www.freescale.com/mqx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;After installation, the USB HID Device example projects (Mouse and CW10 for example) could be found on the&lt;BR /&gt;following path:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; C:\Freescale\Freescale_MQX_4_0\usb\device\examples\hid\mouse\cw10\hid_mouse_dev_twrk60f120m\&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 01:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234222#M5327</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2013-04-10T01:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60F+USB Stack</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234223#M5328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello, thank you for the answer, I'm already using the usb stack examples of HID app, and it works but only with the twr-ser, but with the Twr-ser2, i cant get that the computer renognize ths usb device, I change the code to hability the high speed and do the jumper configuration, but still no luck. Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 13:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60F-USB-Stack/m-p/234223#M5328</guid>
      <dc:creator>xavi2804</dc:creator>
      <dc:date>2013-04-10T13:53:44Z</dc:date>
    </item>
  </channel>
</rss>