<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV42 FTM Fault input error</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV42-FTM-Fault-input-error/m-p/908311#M53276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yu Fuhua,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will suggest to check the pwm_twochannel example that comes in the SDK.&lt;/P&gt;&lt;P&gt;You can download the SDK from this webpage:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2019 23:15:23 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-05-28T23:15:23Z</dc:date>
    <item>
      <title>KV42 FTM Fault input error</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV42-FTM-Fault-input-error/m-p/908310#M53275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying FTM_Fault input to disable the PWM output function. Now I can output normal two channels complementary signal. FTM0_CH0 and FTM0_CH1. Then prepare to use FTM0_FLT1(MKV42F64VLF16, PTC0) to control the FTM disable the output. The Init code as shown below:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Strangely, code run into IRQHandler every time. And PWM outputs normally. I had measure the PTC0's level, it's high. Could help this?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83903i1903BED0BE1BC74D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83906i4719CBEA7BFE1E5E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2019 14:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV42-FTM-Fault-input-error/m-p/908310#M53275</guid>
      <dc:creator>cyesman</dc:creator>
      <dc:date>2019-05-27T14:22:46Z</dc:date>
    </item>
    <item>
      <title>Re: KV42 FTM Fault input error</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV42-FTM-Fault-input-error/m-p/908311#M53276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Yu Fuhua,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will suggest to check the pwm_twochannel example that comes in the SDK.&lt;/P&gt;&lt;P&gt;You can download the SDK from this webpage:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 23:15:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV42-FTM-Fault-input-error/m-p/908311#M53276</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-05-28T23:15:23Z</dc:date>
    </item>
  </channel>
</rss>