<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kinetis Drivers - fsl_flash versus fsl_ftfx_flash in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Drivers-fsl-flash-versus-fsl-ftfx-flash/m-p/903474#M53100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see that some of the demos and/or examples use the &lt;STRONG&gt;fsl_flash&lt;/STRONG&gt; driver, and others use the &lt;STRONG&gt;fsl_ftfx_flash&lt;/STRONG&gt; driiver.&amp;nbsp; At first glance the APIs look the same.&amp;nbsp; However, the underlying code is different.&amp;nbsp; For example, fsl_flash has a mechanism to copy and execute the driver functions from RAM, which is not present in fsl_ftfx_flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is preferred?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Apr 2019 23:33:57 GMT</pubDate>
    <dc:creator>deniscollis</dc:creator>
    <dc:date>2019-04-19T23:33:57Z</dc:date>
    <item>
      <title>Kinetis Drivers - fsl_flash versus fsl_ftfx_flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Drivers-fsl-flash-versus-fsl-ftfx-flash/m-p/903474#M53100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see that some of the demos and/or examples use the &lt;STRONG&gt;fsl_flash&lt;/STRONG&gt; driver, and others use the &lt;STRONG&gt;fsl_ftfx_flash&lt;/STRONG&gt; driiver.&amp;nbsp; At first glance the APIs look the same.&amp;nbsp; However, the underlying code is different.&amp;nbsp; For example, fsl_flash has a mechanism to copy and execute the driver functions from RAM, which is not present in fsl_ftfx_flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is preferred?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 23:33:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Drivers-fsl-flash-versus-fsl-ftfx-flash/m-p/903474#M53100</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2019-04-19T23:33:57Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Drivers - fsl_flash versus fsl_ftfx_flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Drivers-fsl-flash-versus-fsl-ftfx-flash/m-p/903475#M53101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis Collis,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; fsl_ftfx also copy the run command to ram, please check this code:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80088iEBE42ADD874A7802/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you use the flash, please copy the launch command code to RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2019 05:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Drivers-fsl-flash-versus-fsl-ftfx-flash/m-p/903475#M53101</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-04-22T05:29:56Z</dc:date>
    </item>
  </channel>
</rss>