<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Change QSPI Boot Entry-Point on K8x</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Change-QSPI-Boot-Entry-Point-on-K8x/m-p/903444#M53099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently faced this problem as FCA and BCA are appended as defined in IAR, External Flash has Two ranges A and B or( QSPI A and QSPI B) where you can map these as two independent application, but a jump to the other can only be possible if its been hard-coded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As entry point change will require changes in VCTOR register of SCB of arm(To Remap Interrrupt Vector Table).&lt;/P&gt;&lt;P&gt;It depends what type of requirement you have in hand.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case I used a Second Stage Bootloader to move entry points in FCA and BCA region, as initial FCA and BCA region are required during initial boot only, a Second Stage Loader/Application can update Them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Saurabh Saxena&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Apr 2019 18:56:25 GMT</pubDate>
    <dc:creator>saurabhsaxena</dc:creator>
    <dc:date>2019-04-19T18:56:25Z</dc:date>
    <item>
      <title>Change QSPI Boot Entry-Point on K8x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Change-QSPI-Boot-Entry-Point-on-K8x/m-p/903443#M53098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to explore the&amp;nbsp;possibility for the K8x MCU to quickly boot into different applications, as needed. This is possible&amp;nbsp;if switching between two applications: one in internal flash, and the other in external QSPI flash.&amp;nbsp; But can I switch between applications that are both on external flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will QSPI Flash offset 0 (mapped address 0x68000000 for the K8x) always be used as the entry point when booting from QSPI XiP Flash?&amp;nbsp; Or is there a way to change the entry point to some other offset in flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could not see anything obvious in BCA , &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Flash Configuration Field&lt;/SPAN&gt;, or QCB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 17:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Change-QSPI-Boot-Entry-Point-on-K8x/m-p/903443#M53098</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2019-04-19T17:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: Change QSPI Boot Entry-Point on K8x</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Change-QSPI-Boot-Entry-Point-on-K8x/m-p/903444#M53099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently faced this problem as FCA and BCA are appended as defined in IAR, External Flash has Two ranges A and B or( QSPI A and QSPI B) where you can map these as two independent application, but a jump to the other can only be possible if its been hard-coded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As entry point change will require changes in VCTOR register of SCB of arm(To Remap Interrrupt Vector Table).&lt;/P&gt;&lt;P&gt;It depends what type of requirement you have in hand.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case I used a Second Stage Bootloader to move entry points in FCA and BCA region, as initial FCA and BCA region are required during initial boot only, a Second Stage Loader/Application can update Them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Saurabh Saxena&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 18:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Change-QSPI-Boot-Entry-Point-on-K8x/m-p/903444#M53099</guid>
      <dc:creator>saurabhsaxena</dc:creator>
      <dc:date>2019-04-19T18:56:25Z</dc:date>
    </item>
  </channel>
</rss>