<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K82: MPU power management</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-power-management/m-p/900057#M53000</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;1. When MPU work, it has power consumption. But there is no such day. I think it is according to how it access the protected area.&lt;/P&gt;&lt;P&gt;2. MPU module needn't clock. When XBS stop, it also stop. It will not dissipate power in low power stop mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 05 May 2019 09:31:50 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-05-05T09:31:50Z</dc:date>
    <item>
      <title>K82: MPU power management</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-power-management/m-p/900056#M52999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see that amount of used MPU regions has effect to power consumption:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Disabling the MPU by clearing CESR[VLD] minimizes power dissipation. To minimize&lt;BR /&gt;the power dissipation of an enabled MPU, invalidate unused region descriptors by&lt;BR /&gt;clearing the associated RGDn_Word3[VLD] bits.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How large effect for power consumption are ?&lt;/P&gt;&lt;P&gt;Does this valid for RUN mode or even in LLS3 mode can be some effect ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 06:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-power-management/m-p/900056#M52999</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-05-03T06:14:31Z</dc:date>
    </item>
    <item>
      <title>Re: K82: MPU power management</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-power-management/m-p/900057#M53000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;1. When MPU work, it has power consumption. But there is no such day. I think it is according to how it access the protected area.&lt;/P&gt;&lt;P&gt;2. MPU module needn't clock. When XBS stop, it also stop. It will not dissipate power in low power stop mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 May 2019 09:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-power-management/m-p/900057#M53000</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-05-05T09:31:50Z</dc:date>
    </item>
  </channel>
</rss>