<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHow to unlock K64F on TWRK64F120M?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-unlock-K64F-on-TWRK64F120M/m-p/899938#M52994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. Without playing with security, the K64F got into a read protected mode. That's from JLink tool with J-Link OpenSDA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connecting to target via SWD&lt;BR /&gt;InitTarget()&lt;BR /&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;BR /&gt;For debugger connection the device needs to be unsecured.&lt;BR /&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;BR /&gt;Device will be unsecured now.&lt;BR /&gt;Timeout while unsecuring device. Erase never starts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Web Chat suggested to try P&amp;amp;E Recovery Tool. However, after putting PE firmware on the OpenSDA, the recovery tool couldn't find the&amp;nbsp;board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd also like to try with my J-Link Plus, but I couldn't figure out what configuration is needed to use it asides from pluggin the ARM Cortex M connector into the K64 JTAG header J5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 May 2019 08:48:00 GMT</pubDate>
    <dc:creator>matthias2</dc:creator>
    <dc:date>2019-05-20T08:48:00Z</dc:date>
    <item>
      <title>How to unlock K64F on TWRK64F120M?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-unlock-K64F-on-TWRK64F120M/m-p/899938#M52994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. Without playing with security, the K64F got into a read protected mode. That's from JLink tool with J-Link OpenSDA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connecting to target via SWD&lt;BR /&gt;InitTarget()&lt;BR /&gt;Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.&lt;BR /&gt;For debugger connection the device needs to be unsecured.&lt;BR /&gt;Note: Unsecuring will trigger a mass erase of the internal flash.&lt;BR /&gt;Device will be unsecured now.&lt;BR /&gt;Timeout while unsecuring device. Erase never starts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Web Chat suggested to try P&amp;amp;E Recovery Tool. However, after putting PE firmware on the OpenSDA, the recovery tool couldn't find the&amp;nbsp;board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd also like to try with my J-Link Plus, but I couldn't figure out what configuration is needed to use it asides from pluggin the ARM Cortex M connector into the K64 JTAG header J5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any other ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 08:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-unlock-K64F-on-TWRK64F120M/m-p/899938#M52994</guid>
      <dc:creator>matthias2</dc:creator>
      <dc:date>2019-05-20T08:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: How to unlock K64F on TWRK64F120M?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-unlock-K64F-on-TWRK64F120M/m-p/899939#M52995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks to this answer&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/503271"&gt;How to use external J-Link Plus with TWRK64F?&lt;/A&gt;, I was able to connect a J-Link Plus externally. Then,&amp;nbsp;I've used the GUI Flash tool in MCUXpresso with the J-Link, and selected the "Resurrect locked Kinetis device", which worked the first time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, in my setup, I was (only) able to unlock it using an external J-Link Plus.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 09:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-unlock-K64F-on-TWRK64F120M/m-p/899939#M52995</guid>
      <dc:creator>matthias2</dc:creator>
      <dc:date>2019-05-20T09:35:19Z</dc:date>
    </item>
  </channel>
</rss>