<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックAnybody added external SRAM to Kinetis K60 while using MQX.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233562#M5294</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is anybody running MQX on a K60 processor with external SRAM?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I am exhausting RAM, which manifests itself when TCP sockets are opened. Currently only have about 20K free when the application is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the question is really how easy will it be to add external sram and make MQX aware/use it. (Also any idea if there is a performance hit?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 May 2013 07:16:51 GMT</pubDate>
    <dc:creator>grixk60n512</dc:creator>
    <dc:date>2013-05-10T07:16:51Z</dc:date>
    <item>
      <title>Anybody added external SRAM to Kinetis K60 while using MQX.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233562#M5294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is anybody running MQX on a K60 processor with external SRAM?&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I am exhausting RAM, which manifests itself when TCP sockets are opened. Currently only have about 20K free when the application is running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the question is really how easy will it be to add external sram and make MQX aware/use it. (Also any idea if there is a performance hit?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 07:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233562#M5294</guid>
      <dc:creator>grixk60n512</dc:creator>
      <dc:date>2013-05-10T07:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: Anybody added external SRAM to Kinetis K60 while using MQX.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233563#M5295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I've done it. I'm the hardware guy, so I'm not up to speed with all the MQX issues, but basically we hung 1Mx16 SRAM on the Flexbus and used FB_CS3 to decode it. It works better if you don't mix up your BHE and BLE strobes. With 70nsec SRAM we needed 4 wait states with a 50MHz Flexbus clock, so there is a performance penalty. You haven't specified which K60 you are using as the subfamily 3 parts will cache the SRAM and the subfamily 2 parts wont.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think the MQX bit was too difficult. I think you just need to edit your .icf and rebuild your BSP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2013 14:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233563#M5295</guid>
      <dc:creator>OliverSedlacek</dc:creator>
      <dc:date>2013-05-13T14:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: Anybody added external SRAM to Kinetis K60 while using MQX.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233564#M5296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oliver,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm the software guy :smileyhappy:, and I thought as much re : the changes to the linker file. Will pass on the info to the hardware guy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a ton.&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 04:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Anybody-added-external-SRAM-to-Kinetis-K60-while-using-MQX/m-p/233564#M5296</guid>
      <dc:creator>grixk60n512</dc:creator>
      <dc:date>2013-05-14T04:58:02Z</dc:date>
    </item>
  </channel>
</rss>