<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KDS 3.2.0 - issue with linker gone missing</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897983#M52932</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to migrate an older KL03 KDS project to a new computer and having a strange issue.&amp;nbsp;&amp;nbsp; Under "properties -&amp;gt; C/C++ build --&amp;gt; Settings --&amp;gt; Tool Settings" the "cross ARM C Linker" has gone missing and not sure what to make of it.&amp;nbsp; &lt;/P&gt;&lt;P&gt;With the same KDS 3.2.0 environment, we can bring in a K64 project and all is well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are details of the KL03 project:&lt;/P&gt;&lt;P&gt;1. It is using KSDK_1.3.0&amp;nbsp;&amp;nbsp; library&lt;/P&gt;&lt;P&gt;2. Using KDS 3.2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am aware that if the build artifact type is set to anything other than executable the linker in the tool settings tab will go away.&amp;nbsp;&amp;nbsp; And, given that other projects seem to work fine, I think there is something either with KDS installation or the project itself or maybe installed software missing (Help-&amp;gt;Installation Details)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 May 2019 14:18:40 GMT</pubDate>
    <dc:creator>aes_mike</dc:creator>
    <dc:date>2019-05-01T14:18:40Z</dc:date>
    <item>
      <title>KDS 3.2.0 - issue with linker gone missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897983#M52932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to migrate an older KL03 KDS project to a new computer and having a strange issue.&amp;nbsp;&amp;nbsp; Under "properties -&amp;gt; C/C++ build --&amp;gt; Settings --&amp;gt; Tool Settings" the "cross ARM C Linker" has gone missing and not sure what to make of it.&amp;nbsp; &lt;/P&gt;&lt;P&gt;With the same KDS 3.2.0 environment, we can bring in a K64 project and all is well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are details of the KL03 project:&lt;/P&gt;&lt;P&gt;1. It is using KSDK_1.3.0&amp;nbsp;&amp;nbsp; library&lt;/P&gt;&lt;P&gt;2. Using KDS 3.2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am aware that if the build artifact type is set to anything other than executable the linker in the tool settings tab will go away.&amp;nbsp;&amp;nbsp; And, given that other projects seem to work fine, I think there is something either with KDS installation or the project itself or maybe installed software missing (Help-&amp;gt;Installation Details)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 14:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897983#M52932</guid>
      <dc:creator>aes_mike</dc:creator>
      <dc:date>2019-05-01T14:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: KDS 3.2.0 - issue with linker gone missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897984#M52933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if I can follow, so can you share a screenshot what you see?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 14:31:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897984#M52933</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-05-01T14:31:58Z</dc:date>
    </item>
    <item>
      <title>Re: KDS 3.2.0 - issue with linker gone missing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897985#M52934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the vagueness.&amp;nbsp; We are working with a customer off-site trying to get them setup with KDS for an older project.&amp;nbsp; I will try to get more information.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 20:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KDS-3-2-0-issue-with-linker-gone-missing/m-p/897985#M52934</guid>
      <dc:creator>aes_mike</dc:creator>
      <dc:date>2019-05-01T20:38:25Z</dc:date>
    </item>
  </channel>
</rss>