<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックQuestions on MKL26Z128CAL4R</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Questions-on-MKL26Z128CAL4R/m-p/897244#M52899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm interested in using&amp;nbsp;MKL26Z128CAL4R, have a few questions,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. From the DS, it seems that VDDA has to be the same voltage as VDD?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;- Can VDD = 1.8V, VDDA =&amp;nbsp; 3.3V supported?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- If VDDA and VDD = 3.3V, can I2C still operate normally at &lt;A href="mailto:PUR@1.8V?"&gt;PUR@1.8V?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I see that VREFH and VREFL is tied to VDDA/VSSA, and unlike most other Kinetis, this one do not have VREF_Out pin,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - Can I use internal bandgap (1.2V) as vref for the SAR ADC?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - Can I use external VREF (from another chip) as ADC VREF?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I only need to use the ADC, DAC and MCU. Can I use the MCU with only internal OSC (no XTAL)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Apr 2019 23:21:36 GMT</pubDate>
    <dc:creator>pchong</dc:creator>
    <dc:date>2019-04-30T23:21:36Z</dc:date>
    <item>
      <title>Questions on MKL26Z128CAL4R</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Questions-on-MKL26Z128CAL4R/m-p/897244#M52899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm interested in using&amp;nbsp;MKL26Z128CAL4R, have a few questions,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. From the DS, it seems that VDDA has to be the same voltage as VDD?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;- Can VDD = 1.8V, VDDA =&amp;nbsp; 3.3V supported?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- If VDDA and VDD = 3.3V, can I2C still operate normally at &lt;A href="mailto:PUR@1.8V?"&gt;PUR@1.8V?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I see that VREFH and VREFL is tied to VDDA/VSSA, and unlike most other Kinetis, this one do not have VREF_Out pin,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - Can I use internal bandgap (1.2V) as vref for the SAR ADC?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; - Can I use external VREF (from another chip) as ADC VREF?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;3. I only need to use the ADC, DAC and MCU. Can I use the MCU with only internal OSC (no XTAL)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2019 23:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Questions-on-MKL26Z128CAL4R/m-p/897244#M52899</guid>
      <dc:creator>pchong</dc:creator>
      <dc:date>2019-04-30T23:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: Questions on MKL26Z128CAL4R</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Questions-on-MKL26Z128CAL4R/m-p/897245#M52900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hello,&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;1.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;-Not supported.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;-No, since the I2C will work with a voltage level of 3.3, so a high is around 0.7VDD = 0.7*3.3 = 2.31V minimum, for this you can use an I2C voltage level translator, for example &lt;A href="https://www.nxp.com/products/analog/voltage-level-translators/dual-supply-translating-transceiver-open-drain-auto-direction-sensing:NTS0102"&gt;NTS0102 &lt;/A&gt;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;2.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Yes, you can use the Vref from another source, but VREFH should be higher than VDDA and VREFL should be at the same voltage potential as VSSA.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;3.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Yes , you shouldn't have a problem using the ADC &amp;amp; DAC.&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Hope this helps,&lt;/P&gt;&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;Regards,&lt;BR /&gt; Aldo.&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 May 2019 21:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Questions-on-MKL26Z128CAL4R/m-p/897245#M52900</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2019-05-03T21:15:41Z</dc:date>
    </item>
  </channel>
</rss>