<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Which .board file is correct for FRDM-K20D50M?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233549#M5285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks David, Just uncheck? Good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I found an answer from Kan Li in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/306270"&gt;https://community.freescale.com/thread/306270&lt;/A&gt; He suggested to use &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;FlashK60Dxxx16K.board&lt;/SPAN&gt;. And offer an update file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I would like to suggest FSL to hire or assign extra test/verification engineer to test the package before release. It saves a lot in following support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jan 2014 00:03:04 GMT</pubDate>
    <dc:creator>kai_liu</dc:creator>
    <dc:date>2014-01-15T00:03:04Z</dc:date>
    <item>
      <title>Which .board file is correct for FRDM-K20D50M?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233547#M5283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have one FRDM-K20D50M at hand. IAR is my preferred compiler, but it reports following error when I invoke its debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Missing or malformed flash loader specification file: C:\Program Files\IAR Systems\Embedded Workbench 6.5\arm\config\flashloader\Freescale\FlashK20Xxxx.board&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems FlashK20Xxxx.board is missing in that directory, neither in IAR 6.5 or latest IAR 6.7. I suppose it is a legacy one used in 6.2/6.3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the replacement. There are some candidates. &lt;STRONG&gt;Which one is suitable for MK20DX128VLH5 on board?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FlashKMxx128K.board&lt;/P&gt;&lt;P&gt;FlashKx0Dxxx128K_2K_1K.board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 12:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233547#M5283</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-01-14T12:26:55Z</dc:date>
    </item>
    <item>
      <title>Re: Which .board file is correct for FRDM-K20D50M?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233548#M5284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kai,&lt;/P&gt;&lt;P&gt;Please open the project "Options" menu:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_48 Jan. 14 09.37.gif"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42358iF332E65D009FC752/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_48 Jan. 14 09.37.gif" alt="ScreenHunter_48 Jan. 14 09.37.gif" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then un-check "Overrride default .board file":&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ScreenHunter_49 Jan. 14 09.38.gif"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42359iF3DEF1FE74879E57/image-size/large?v=v2&amp;amp;px=999" role="button" title="ScreenHunter_49 Jan. 14 09.38.gif" alt="ScreenHunter_49 Jan. 14 09.38.gif" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 15:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233548#M5284</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-01-14T15:41:47Z</dc:date>
    </item>
    <item>
      <title>Re: Which .board file is correct for FRDM-K20D50M?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233549#M5285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks David, Just uncheck? Good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I found an answer from Kan Li in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/306270"&gt;https://community.freescale.com/thread/306270&lt;/A&gt; He suggested to use &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;FlashK60Dxxx16K.board&lt;/SPAN&gt;. And offer an update file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I would like to suggest FSL to hire or assign extra test/verification engineer to test the package before release. It saves a lot in following support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jan 2014 00:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-board-file-is-correct-for-FRDM-K20D50M/m-p/233549#M5285</guid>
      <dc:creator>kai_liu</dc:creator>
      <dc:date>2014-01-15T00:03:04Z</dc:date>
    </item>
  </channel>
</rss>