<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 could not find core in coresight setup</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891704#M52701</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using Segger J-Flash v6.32g, processor MK22FN1M0VLH12. J-Flash Target Connect shows (in the log)&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;&amp;nbsp;- Connecting via USB to J-Link device 0&lt;BR /&gt;&amp;nbsp;- Target interface speed: 4000 kHz (Fixed)&lt;BR /&gt;&amp;nbsp;- VTarget = 3.325V&lt;BR /&gt;&amp;nbsp;- ERROR: Could not find core in Coresight setup&lt;BR /&gt;&amp;nbsp;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Apr 2019 17:31:50 GMT</pubDate>
    <dc:creator>albertdoe</dc:creator>
    <dc:date>2019-04-10T17:31:50Z</dc:date>
    <item>
      <title>could not find core in coresight setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891704#M52701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using Segger J-Flash v6.32g, processor MK22FN1M0VLH12. J-Flash Target Connect shows (in the log)&lt;/P&gt;&lt;P&gt;Connecting ...&lt;BR /&gt;&amp;nbsp;- Connecting via USB to J-Link device 0&lt;BR /&gt;&amp;nbsp;- Target interface speed: 4000 kHz (Fixed)&lt;BR /&gt;&amp;nbsp;- VTarget = 3.325V&lt;BR /&gt;&amp;nbsp;- ERROR: Could not find core in Coresight setup&lt;BR /&gt;&amp;nbsp;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2019 17:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891704#M52701</guid>
      <dc:creator>albertdoe</dc:creator>
      <dc:date>2019-04-10T17:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: could not find core in coresight setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891705#M52702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Albert,&lt;/P&gt;&lt;P&gt;If there is no other hardware issue, I guess your chip is locked. Please see this link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/1013892"&gt;https://community.nxp.com/message/1013892&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 07:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891705#M52702</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-04-11T07:45:47Z</dc:date>
    </item>
    <item>
      <title>Re: could not find core in coresight setup</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891706#M52703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a K60DN512VLL10 and I encountered the same "could not find core in coresight setup" problem.&lt;/P&gt;&lt;P&gt;I'm using Segger V6.56B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I connected with J-Link Commander V6.56b to attempt to unlock my core as suggested by Jing, and the command tool is unable to connect.&lt;/P&gt;&lt;P&gt;It appears to unlock with success but cannot erase.&amp;nbsp; It encounters the same problem:Could not find core in Coresight setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide other suggestions?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/83765iA14BB9282C28C31D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2020 16:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/could-not-find-core-in-coresight-setup/m-p/891706#M52703</guid>
      <dc:creator>tbiberdorf</dc:creator>
      <dc:date>2020-03-05T16:58:49Z</dc:date>
    </item>
  </channel>
</rss>