<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K82 : MPU advanced features ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-advanced-features/m-p/890239#M52614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just wondering if possible to assign some separate access rights to interrupt handlers&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;They run in privileged mode only and if they running when specific rtos task context is valid, it means full access to&amp;nbsp;&lt;/P&gt;&lt;P&gt;task's memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to have memory chunks what visible only when task is active. In other time no user/privileged access at all.&lt;/P&gt;&lt;P&gt;Or only one way is exists is to disable task's specific MPU regions at beginning of ISR and return back at the end of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or other technique is exists for utilise K82 MPU for this case ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2019 12:13:25 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2019-04-24T12:13:25Z</dc:date>
    <item>
      <title>K82 : MPU advanced features ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-advanced-features/m-p/890239#M52614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just wondering if possible to assign some separate access rights to interrupt handlers&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;They run in privileged mode only and if they running when specific rtos task context is valid, it means full access to&amp;nbsp;&lt;/P&gt;&lt;P&gt;task's memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to have memory chunks what visible only when task is active. In other time no user/privileged access at all.&lt;/P&gt;&lt;P&gt;Or only one way is exists is to disable task's specific MPU regions at beginning of ISR and return back at the end of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or other technique is exists for utilise K82 MPU for this case ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 12:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-advanced-features/m-p/890239#M52614</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-04-24T12:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : MPU advanced features ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-advanced-features/m-p/890240#M52615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can only fully access the NVIC from privileged mode. I think the only way to do this behavior is by disabling MPU section during the ISR.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2019 16:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-MPU-advanced-features/m-p/890240#M52615</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-04-26T16:45:29Z</dc:date>
    </item>
  </channel>
</rss>