<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB/VREG pins on the K66 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-VREG-pins-on-the-K66/m-p/885506#M52422</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have&amp;nbsp;a similar question to that which was posed in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/433535"&gt;this forum post&lt;/A&gt; but was never directly answered:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I'm using the USB DP/DM pins on the K66 (pins 19 and 20) but don't need the K66's USB regulator (VREG), can I just tie the VREG_INx pins to my schematic's externally regulated +3.3V supply along with VREG_OUT? The &lt;A href="https://www.nxp.com/docs/en/data-sheet/K66P144M180SF5V2.pdf"&gt;datasheet &lt;/A&gt;specifies what to do with the pins if the USB function isn't used at all, but it's unclear what to do with them if I want to use USB communication but don't want to use the internal USB regulator.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Feb 2019 22:00:30 GMT</pubDate>
    <dc:creator>matthew_trowbri</dc:creator>
    <dc:date>2019-02-05T22:00:30Z</dc:date>
    <item>
      <title>USB/VREG pins on the K66</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-VREG-pins-on-the-K66/m-p/885506#M52422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have&amp;nbsp;a similar question to that which was posed in &lt;A _jive_internal="true" href="https://community.nxp.com/thread/433535"&gt;this forum post&lt;/A&gt; but was never directly answered:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I'm using the USB DP/DM pins on the K66 (pins 19 and 20) but don't need the K66's USB regulator (VREG), can I just tie the VREG_INx pins to my schematic's externally regulated +3.3V supply along with VREG_OUT? The &lt;A href="https://www.nxp.com/docs/en/data-sheet/K66P144M180SF5V2.pdf"&gt;datasheet &lt;/A&gt;specifies what to do with the pins if the USB function isn't used at all, but it's unclear what to do with them if I want to use USB communication but don't want to use the internal USB regulator.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 22:00:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-VREG-pins-on-the-K66/m-p/885506#M52422</guid>
      <dc:creator>matthew_trowbri</dc:creator>
      <dc:date>2019-02-05T22:00:30Z</dc:date>
    </item>
    <item>
      <title>Re: USB/VREG pins on the K66</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-VREG-pins-on-the-K66/m-p/885507#M52423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, I think it is no problem. Figure 53-1 in RM shows that VREGOUT connects USB-FS and USB-HS. And When you add 3.3V to VREGIN0, it will work in pass-through mode. I test your idea on a TWR-K65 board. I disconnect J23, connect J23-2 to 3.3v and connect J9-7 with J9-8. It works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 05:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-VREG-pins-on-the-K66/m-p/885507#M52423</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-02-13T05:55:24Z</dc:date>
    </item>
  </channel>
</rss>