<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MSCAN CRC on CAN Message</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883488#M52378</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harish Shekarappa,&lt;/P&gt;&lt;P&gt;You don't need to manually calculate the CRC and add to the Frame buffer.&lt;/P&gt;&lt;P&gt;About the software, you can download the latest &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;MCUXpresso SDK&lt;/A&gt;.&lt;BR /&gt;I don't know which Kinetis MCU are you using. If KE06 or KE16 are used, please refer the CAN examples in SDK_2.5.0_FRDM-KE06Z or SDK_2.5.0_FRDM-KE16Z.&lt;BR /&gt;...\SDK_2.5.0_FRDM-KE16Z\boards\frdmke16z\driver_examples\mscan\interrupt_transfer&lt;BR /&gt;...\SDK_2.5.0_FRDM-KE06Z\boards\frdmke06z\driver_examples\mscan\loopback_transfer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Apr 2019 03:30:26 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2019-04-12T03:30:26Z</dc:date>
    <item>
      <title>MSCAN CRC on CAN Message</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883486#M52376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MSCAN CAN example CAN_CheckSendBufferFrame transmits the Data on the CAN bus, I wanted to know whether the CAN message is sent with CRC? or do we need to manually calculate the CRC and add to the&amp;nbsp;Frame buffer?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2019 23:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883486#M52376</guid>
      <dc:creator>harish_shekarap</dc:creator>
      <dc:date>2019-04-05T23:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN CRC on CAN Message</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883487#M52377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CRC is generated in the HW on transmission and check in the HW in reception. I don't think that any CAN controller will require it to be done in SW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Apr 2019 15:47:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883487#M52377</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-04-07T15:47:37Z</dc:date>
    </item>
    <item>
      <title>Re: MSCAN CRC on CAN Message</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883488#M52378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Harish Shekarappa,&lt;/P&gt;&lt;P&gt;You don't need to manually calculate the CRC and add to the Frame buffer.&lt;/P&gt;&lt;P&gt;About the software, you can download the latest &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;MCUXpresso SDK&lt;/A&gt;.&lt;BR /&gt;I don't know which Kinetis MCU are you using. If KE06 or KE16 are used, please refer the CAN examples in SDK_2.5.0_FRDM-KE06Z or SDK_2.5.0_FRDM-KE16Z.&lt;BR /&gt;...\SDK_2.5.0_FRDM-KE16Z\boards\frdmke16z\driver_examples\mscan\interrupt_transfer&lt;BR /&gt;...\SDK_2.5.0_FRDM-KE06Z\boards\frdmke06z\driver_examples\mscan\loopback_transfer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2019 03:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MSCAN-CRC-on-CAN-Message/m-p/883488#M52378</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-04-12T03:30:26Z</dc:date>
    </item>
  </channel>
</rss>