<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Why Kinetis Microcontroller crashed?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Kinetis-Microcontroller-crashed/m-p/883062#M52373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gabriele,&lt;/P&gt;&lt;P&gt;No, there isn't such a protection circuit. But in K22 SDK, there is a power switch demo. It shows how to step into and release from all of the power mode, both by wakeup pin and timer. You can refer to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Apr 2019 08:18:07 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-04-08T08:18:07Z</dc:date>
    <item>
      <title>Why Kinetis Microcontroller crashed?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Kinetis-Microcontroller-crashed/m-p/883061#M52372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a MK22FX512AVLL12. I have selected LLWU_P15 used like interrupt to wake up the microcontroller.&lt;/P&gt;&lt;P&gt;During normal use I reach some unknown bug in my huge code but the microcontroller reaches a condition i can't understand.&lt;/P&gt;&lt;P&gt;All the GPIO are disabled, the microcontroller seems in sleep. But the wakeup interrupt doesn't wake&amp;nbsp; up the micro, and the code doesn't restart automatically (watchdog is active, should do it). Only a reset make it waking up.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is some protection circuit that could stop the microcontroller in this way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gabriele&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2019 11:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Kinetis-Microcontroller-crashed/m-p/883061#M52372</guid>
      <dc:creator>gabriele_endriz</dc:creator>
      <dc:date>2019-04-05T11:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Why Kinetis Microcontroller crashed?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Kinetis-Microcontroller-crashed/m-p/883062#M52373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gabriele,&lt;/P&gt;&lt;P&gt;No, there isn't such a protection circuit. But in K22 SDK, there is a power switch demo. It shows how to step into and release from all of the power mode, both by wakeup pin and timer. You can refer to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 08:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Kinetis-Microcontroller-crashed/m-p/883062#M52373</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-04-08T08:18:07Z</dc:date>
    </item>
  </channel>
</rss>