<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL27Z I2C ACK PROBLEM in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z-I2C-ACK-PROBLEM/m-p/881984#M52308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will need to set the pins as open drain using the internal pull resistor. This can be configured with the &lt;STRONG&gt;PORTx_PCRn &lt;/STRONG&gt;register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL27P64M48SF6RM.pdf"&gt;reference manual&lt;/A&gt; in section 11.7.1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Feb 2019 23:09:59 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2019-02-08T23:09:59Z</dc:date>
    <item>
      <title>KL27Z I2C ACK PROBLEM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z-I2C-ACK-PROBLEM/m-p/881983#M52307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm working on a project and i have to use an EEPROM and a KL27Z256 microcontroller.&lt;/P&gt;&lt;P&gt;The problem is when the slave(the EEPROM) sends the ACK bit. It only goes half way down. I've been searching about this, and i know that i have to put the SDA line in open collector. But in this microcontroller there's no register to do that.&lt;/P&gt;&lt;P&gt;I need information about how to do this.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Jose Ricaurte Pino&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2019 21:43:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z-I2C-ACK-PROBLEM/m-p/881983#M52307</guid>
      <dc:creator>jricaurtepino</dc:creator>
      <dc:date>2019-02-04T21:43:46Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z I2C ACK PROBLEM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z-I2C-ACK-PROBLEM/m-p/881984#M52308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will need to set the pins as open drain using the internal pull resistor. This can be configured with the &lt;STRONG&gt;PORTx_PCRn &lt;/STRONG&gt;register.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please refer to the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL27P64M48SF6RM.pdf"&gt;reference manual&lt;/A&gt; in section 11.7.1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Feb 2019 23:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z-I2C-ACK-PROBLEM/m-p/881984#M52308</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-02-08T23:09:59Z</dc:date>
    </item>
  </channel>
</rss>