<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 USB HID - Keyboard Mouse Examples</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-HID-Keyboard-Mouse-Examples/m-p/880821#M52244</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using two boards one running the keyboard and mouse host examples and one running the keyboard and mouse device examples. Unfortunately, the device examples are set up to constantly output data from the mouse or keyboard device.&amp;nbsp; When I plug the boards together I see a stream of data from the keyboard / mouse HID eval board on my host eval board.&amp;nbsp; If I plug in an actual keyboard to my hose eval board I only see data when I press a key.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I make the device eval board behave this way?&amp;nbsp; When it is plugged into the host eval board the USB_DeviceHidKeyboardCallback is constantly being executed and it appears that it must result in a&amp;nbsp;USB_DeviceHidSend call to function properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I plug an real keyboard in the&amp;nbsp;&lt;SPAN&gt;USB_DeviceHidKeyboardCallback&amp;nbsp;is only executed when I press a key.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I get this behavior in the example code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HID example is the frdmkl27z_dev_composite_hid_mouse_hid_keybaord_bm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 23:55:27 GMT</pubDate>
    <dc:creator>tomtalkington</dc:creator>
    <dc:date>2019-03-21T23:55:27Z</dc:date>
    <item>
      <title>USB HID - Keyboard Mouse Examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-HID-Keyboard-Mouse-Examples/m-p/880821#M52244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using two boards one running the keyboard and mouse host examples and one running the keyboard and mouse device examples. Unfortunately, the device examples are set up to constantly output data from the mouse or keyboard device.&amp;nbsp; When I plug the boards together I see a stream of data from the keyboard / mouse HID eval board on my host eval board.&amp;nbsp; If I plug in an actual keyboard to my hose eval board I only see data when I press a key.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I make the device eval board behave this way?&amp;nbsp; When it is plugged into the host eval board the USB_DeviceHidKeyboardCallback is constantly being executed and it appears that it must result in a&amp;nbsp;USB_DeviceHidSend call to function properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I plug an real keyboard in the&amp;nbsp;&lt;SPAN&gt;USB_DeviceHidKeyboardCallback&amp;nbsp;is only executed when I press a key.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I get this behavior in the example code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HID example is the frdmkl27z_dev_composite_hid_mouse_hid_keybaord_bm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 23:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-HID-Keyboard-Mouse-Examples/m-p/880821#M52244</guid>
      <dc:creator>tomtalkington</dc:creator>
      <dc:date>2019-03-21T23:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: USB HID - Keyboard Mouse Examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-HID-Keyboard-Mouse-Examples/m-p/880822#M52245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The behavior you mention is implemented in &lt;STRONG&gt;USB_DeviceHidKeyboardAction(void)&amp;nbsp;&lt;/STRONG&gt;in hid_keyboard.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take the following code as an example of how you can send data by pressing SW1 and SW3 of your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; usb_status_t &lt;SPAN class="token function"&gt;USB_DeviceHidKeyboardAction&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
 s_UsbDeviceHidKeyboard&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00U&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;g_Button1Press&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  s_UsbDeviceHidKeyboard&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; KEY_A&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="comment token"&gt;/* Reset state of button. */&lt;/SPAN&gt;
  g_Button1Press &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
 &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;g_Button3Press&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
  s_UsbDeviceHidKeyboard&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; KEY_B&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="comment token"&gt;/* Reset state of button. */&lt;/SPAN&gt;
  g_Button3Press &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

 &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;USB_DeviceHidSend&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;s_UsbDeviceComposite&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;hidKeyboardHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; USB_HID_KEYBOARD_ENDPOINT_IN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
   s_UsbDeviceHidKeyboard&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; USB_HID_KEYBOARD_REPORT_LENGTH&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 15:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-HID-Keyboard-Mouse-Examples/m-p/880822#M52245</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-03-26T15:42:00Z</dc:date>
    </item>
  </channel>
</rss>