<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC Fifo in MKE04Z64VLH4 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Fifo-in-MKE04Z64VLH4/m-p/880166#M52222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I want to sample 8 channels of ADC with single command(SW or HW trigger) without any CPU intervention.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Is it possible to use FIFO mode of ADC for this purpose as FIFO mode offloads CPU and gives an interrupt only after sampling of all the ADC channels in ADC channels FIFO has been completed.&lt;/P&gt;&lt;P&gt;Also, is there any sample code that can be used for FIFO operation in MKE04Z64VLH4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 11:29:48 GMT</pubDate>
    <dc:creator>prasannanaik</dc:creator>
    <dc:date>2019-01-17T11:29:48Z</dc:date>
    <item>
      <title>ADC Fifo in MKE04Z64VLH4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Fifo-in-MKE04Z64VLH4/m-p/880166#M52222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I want to sample 8 channels of ADC with single command(SW or HW trigger) without any CPU intervention.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Is it possible to use FIFO mode of ADC for this purpose as FIFO mode offloads CPU and gives an interrupt only after sampling of all the ADC channels in ADC channels FIFO has been completed.&lt;/P&gt;&lt;P&gt;Also, is there any sample code that can be used for FIFO operation in MKE04Z64VLH4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 11:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Fifo-in-MKE04Z64VLH4/m-p/880166#M52222</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-01-17T11:29:48Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Fifo in MKE04Z64VLH4</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Fifo-in-MKE04Z64VLH4/m-p/880167#M52223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Prasanna,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please download the &lt;A href="https://www.nxp.com/webapp/Download?colCode=FRDM-KEXX-Driver-Library-Package&amp;amp;appType=license"&gt;FRDM-KEXX Driver Library Package (REV 2.0).&lt;/A&gt;&lt;BR /&gt;Then you will find the ADC_FIFO_demo.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ADC_FIFO_demo.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63873i73C2A0DE48D73B87/image-size/large?v=v2&amp;amp;px=999" role="button" title="ADC_FIFO_demo.png" alt="ADC_FIFO_demo.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 09:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-Fifo-in-MKE04Z64VLH4/m-p/880167#M52223</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-01-21T09:05:11Z</dc:date>
    </item>
  </channel>
</rss>