<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 TPM timer initial delay when using 32kHz EXTAL</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879394#M52204</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use TPM clock on KL17 using external 32kHz crystal. I've initialized MOD value with 32, so expecting it to interrupt after 1ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I always get the first interrupt from tpm counter after 120ms delay, subsequent interrupts happen at 1ms interval.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers to debugging this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Feb 2019 08:50:06 GMT</pubDate>
    <dc:creator>jpatel1</dc:creator>
    <dc:date>2019-02-01T08:50:06Z</dc:date>
    <item>
      <title>TPM timer initial delay when using 32kHz EXTAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879394#M52204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use TPM clock on KL17 using external 32kHz crystal. I've initialized MOD value with 32, so expecting it to interrupt after 1ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I always get the first interrupt from tpm counter after 120ms delay, subsequent interrupts happen at 1ms interval.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers to debugging this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 08:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879394#M52204</guid>
      <dc:creator>jpatel1</dc:creator>
      <dc:date>2019-02-01T08:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: TPM timer initial delay when using 32kHz EXTAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879395#M52205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;How are you measuring the first pulse, remember you will need to add the time for the clock stabilization&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2019 03:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879395#M52205</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-02-07T03:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: TPM timer initial delay when using 32kHz EXTAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879396#M52206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Vincente for the response!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using gpio pin toggle when I initialize TPM timer and when I receive interrupt; measuring the delay using oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is the best way to verify in code if&amp;nbsp;crystal/clock stabilization has happened? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using VLPS3 sleep mode with RTC configured for external crystal. I was expecting the delay will not happen when waking up from sleep as OSC still running in sleep mode. What am I missing here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 22:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TPM-timer-initial-delay-when-using-32kHz-EXTAL/m-p/879396#M52206</guid>
      <dc:creator>jpatel1</dc:creator>
      <dc:date>2019-03-14T22:31:57Z</dc:date>
    </item>
  </channel>
</rss>