<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis K12 Periodic DMA Triggering</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879272#M52194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know that I have used the PIT DMA trigger on a device with this errata but if this is the reason you can switch to using a FlexTimer channel as trigger instead. The FlexTimer can be used to generate a fixed number of pulses at a certain frequency and, using DMA, change the frequency and next step counter at the end of the period to automatically generate stepper motor acceleration/deceleration ramps, etc. and so is potentially more flexible too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Mar 2019 14:05:22 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2019-03-11T14:05:22Z</dc:date>
    <item>
      <title>[SOLVED] Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879268#M52190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use DMA in periodic trigger mode to transfer data from memory to the PDOR register of a port. I've set the source to one of the always-on slots. My expectation is that a minor loop (a byte in my case) transaction would be carried out every time the PIT timer interrupt happens. However, when PIT interrupt fires, all my data (until major loop is completed) is being written to the PDOR without any throttling. What I'm trying to do should be possible according to section 20.4.3 of the reference manual. Could you please point me in the right direction, maybe&amp;nbsp;provide me with an example project that I can use as a reference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;MK12DX128VLF5 on a custom board. I'm using PIT channel 0 with DMA channel 0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best wishes,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 17:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879268#M52190</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2019-03-08T17:15:56Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879269#M52191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Set DREQ in DMA_TCDx_CSR to get a single transfer for each trigger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of continued difficulties just use the open source uTasker solution on GitHub which support this in its PIT driver as follows (DMA channel is always DMAMUX0 for PIT0 and DMAMUX1 for PIT1):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;PIT_SETUP pit_setup&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                                 &lt;SPAN class="comment token"&gt;// PIT interrupt configuration parameters&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_type &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PIT_INTERRUPT&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;mode &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;PIT_PERIODIC &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; PIT_OUTPUT_DMA_TRIG&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;               &lt;SPAN class="comment token"&gt;// periodic with DMA trigger to control a port toggle&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;int_handler &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                           &lt;SPAN class="comment token"&gt;// no interrupt due to DM&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;count_delay &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;PIT_US_DELAY&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                             &lt;SPAN class="comment token"&gt;// 1us period (for 500kHz square wave)&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;ucPIT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                                 &lt;SPAN class="comment token"&gt;// use PIT0&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;ulPortBits &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORTA_BIT1&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                                   &lt;SPAN class="comment token"&gt;// toggle PTA1 on each PIT trigger&lt;/SPAN&gt;
pit_setup&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;ucPortRef &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PORTA&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;fnConfigureInterrupt&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;pit_setup&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                            &lt;SPAN class="comment token"&gt;// configure PIT&lt;/SPAN&gt;
‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;Complete Kinetis solutions, training and support: &lt;A href="http://www.utasker.com/kinetis.html" rel="nofollow noopener noreferrer" target="test_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 20:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879269#M52191</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-03-08T20:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879270#M52192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, this doesn't fix the issue I'm having.&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;DREQ in DMA_TCDx_CSR is already set. According to the reference manual, setting that bit will make eDMA clear the ERQ bit after a major loop completion. What I'm trying to do is to clear ERQ after a minor loop completion. So basically, I've set the major loop count to 38 bytes and minor to 1 byte. I'm attempting to send the one byte every time PIT interrupt happens until all the 38 bytes are transferred.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best wishes,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Daniel&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 11:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879270#M52192</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2019-03-11T11:05:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879271#M52193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks like it is an issue with the Kinetis MCU. I found this errata e4588&amp;nbsp;&lt;A class="link-titled" href="http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_4N30D.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_4N30D.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/errata/KINETIS_4N30D.pdf&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 12:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879271#M52193</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2019-03-11T12:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879272#M52194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know that I have used the PIT DMA trigger on a device with this errata but if this is the reason you can switch to using a FlexTimer channel as trigger instead. The FlexTimer can be used to generate a fixed number of pulses at a certain frequency and, using DMA, change the frequency and next step counter at the end of the period to automatically generate stepper motor acceleration/deceleration ramps, etc. and so is potentially more flexible too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 14:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879272#M52194</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-03-11T14:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K12 Periodic DMA Triggering</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879273#M52195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yeah that's what I just did and it is working fine with using one FlexTimer channel.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for all your help.&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 14:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SOLVED-Kinetis-K12-Periodic-DMA-Triggering/m-p/879273#M52195</guid>
      <dc:creator>danielberhe</dc:creator>
      <dc:date>2019-03-11T14:08:07Z</dc:date>
    </item>
  </channel>
</rss>