<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUse FRDM-KL25Z as a debug probe.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877485#M52135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It cut J11 as shown in the FRDM-KL25Z user's manual and connected to SWDCLK and SWDDIO of the MCU outside the board.&lt;BR /&gt;The external MCU is MKM14Z64ACHH5.&lt;/P&gt;&lt;P&gt;If you set the debugger to PE-micro from EWARM of IAR and write to flash&lt;BR /&gt;First, when the PEMICRO Connection Manager screen appears and press Connect, an error message appears.&lt;/P&gt;&lt;P&gt;Error 17926. Target Type MCU mismatch. Unexpected processor detected. Aborting debug sesion.&lt;/P&gt;&lt;P&gt;① Does OpenSDA of FRDM-KL25Z check the CPU, and an MCU different from the KL25Z in the board causes an error?&lt;BR /&gt;② Is there a way to avoid this error and erase / write the external MKM14Z64ACHH5?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks for your instruction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jan 2019 06:08:38 GMT</pubDate>
    <dc:creator>jun1</dc:creator>
    <dc:date>2019-01-16T06:08:38Z</dc:date>
    <item>
      <title>Use FRDM-KL25Z as a debug probe.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877485#M52135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It cut J11 as shown in the FRDM-KL25Z user's manual and connected to SWDCLK and SWDDIO of the MCU outside the board.&lt;BR /&gt;The external MCU is MKM14Z64ACHH5.&lt;/P&gt;&lt;P&gt;If you set the debugger to PE-micro from EWARM of IAR and write to flash&lt;BR /&gt;First, when the PEMICRO Connection Manager screen appears and press Connect, an error message appears.&lt;/P&gt;&lt;P&gt;Error 17926. Target Type MCU mismatch. Unexpected processor detected. Aborting debug sesion.&lt;/P&gt;&lt;P&gt;① Does OpenSDA of FRDM-KL25Z check the CPU, and an MCU different from the KL25Z in the board causes an error?&lt;BR /&gt;② Is there a way to avoid this error and erase / write the external MKM14Z64ACHH5?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks for your instruction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 06:08:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877485#M52135</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-01-16T06:08:38Z</dc:date>
    </item>
    <item>
      <title>Re: Use FRDM-KL25Z as a debug probe.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877486#M52136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If using the P&amp;amp;E default firmware, you only can program a microcontroller of the same type, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;Using the Freedom Board as SWD Programmer | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;An option would be to use USBDM, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/" title="https://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/"&gt;Debug External Processors with USBDM and Freedom Board | MCU on Eclipse&lt;/A&gt; , or see here more on this topic: &lt;A class="link-titled" href="https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 17:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877486#M52136</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-01-16T17:48:38Z</dc:date>
    </item>
    <item>
      <title>Re: Use FRDM-KL25Z as a debug probe.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877487#M52137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;BR /&gt;understood.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 23:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-FRDM-KL25Z-as-a-debug-probe/m-p/877487#M52137</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-01-16T23:38:22Z</dc:date>
    </item>
  </channel>
</rss>