<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 	 [USB-KW41Z] Demo gpio_led_output wont seem to work in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW41Z-Demo-gpio-led-output-wont-seem-to-work/m-p/874752#M52037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The default applications in the USB -KW41Z it's the sniffer one, please refer to &lt;A _jive_internal="true" href="https://community.nxp.com/thread/444708"&gt;this&lt;/A&gt; post as it can guide you through the changes needed to use the USB-KW41Z to develop your applications.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt; Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Mar 2019 16:20:41 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2019-03-07T16:20:41Z</dc:date>
    <item>
      <title>[USB-KW41Z] Demo gpio_led_output wont seem to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW41Z-Demo-gpio-led-output-wont-seem-to-work/m-p/874751#M52036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm just getting started with the&amp;nbsp;USB-KW41Z and was trying to get the sample project to blink the LED to work but noting seem to happen. I build it and everything looks good:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building target: usbkw41z_kw41z_driver_examples_gpio_led_output.axf&lt;BR /&gt;Invoking: MCU Linker&lt;BR /&gt;arm-none-eabi-gcc -nostdlib -Xlinker -Map="usbkw41z_kw41z_driver_examples_gpio_led_output.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -mcpu=cortex-m0plus -mthumb -T usbkw41z_kw41z_driver_examples_gpio_led_output_Debug.ld -o "usbkw41z_kw41z_driver_examples_gpio_led_output.axf" ./utilities/fsl_debug_console.o ./startup/startup_mkw41z4.o ./source/gpio_led_output.o ./source/mtb.o ./source/semihost_hardfault.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_flash.o ./drivers/fsl_gpio.o ./drivers/fsl_lptmr.o ./drivers/fsl_lpuart.o ./drivers/fsl_smc.o ./board/board.o ./board/clock_config.o ./board/pin_mux.o ./CMSIS/system_MKW41Z4.o&lt;BR /&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt; PROGRAM_FLASH: 9468 B 512 KB 1.81%&lt;BR /&gt; SRAM: 8536 B 128 KB 6.51%&lt;BR /&gt;Finished building target: usbkw41z_kw41z_driver_examples_gpio_led_output.axf&lt;BR /&gt;&lt;BR /&gt;make --no-print-directory post-build&lt;BR /&gt;Performing post-build steps&lt;BR /&gt;arm-none-eabi-size "usbkw41z_kw41z_driver_examples_gpio_led_output.axf"; # arm-none-eabi-objcopy -v -O binary "usbkw41z_kw41z_driver_examples_gpio_led_output.axf" "usbkw41z_kw41z_driver_examples_gpio_led_output.bin" ; # checksum -p MKW41Z512xxx4 -d "usbkw41z_kw41z_driver_examples_gpio_led_output.bin";&lt;BR /&gt; text data bss dec hex filename&lt;BR /&gt; 9464 4 8532 18000 4650 usbkw41z_kw41z_driver_examples_gpio_led_output.axf&lt;/P&gt;&lt;P&gt;17:52:25 Build Finished (took 9s.586ms)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then hit debug. Select the the device for JLink to connect to and nothing happens&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78956i7F84F96B540D2E7F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The debug window says and looks like everything is OK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i hit the reset OpenSDA button or unplug and re-plug in the device the LED with flash for a few seconds before window connects to the device at which point the led goes solid again. This didn't happen before i programmed it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be great,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 02:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW41Z-Demo-gpio-led-output-wont-seem-to-work/m-p/874751#M52036</guid>
      <dc:creator>csantos</dc:creator>
      <dc:date>2019-03-07T02:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: 	 [USB-KW41Z] Demo gpio_led_output wont seem to work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW41Z-Demo-gpio-led-output-wont-seem-to-work/m-p/874752#M52037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The default applications in the USB -KW41Z it's the sniffer one, please refer to &lt;A _jive_internal="true" href="https://community.nxp.com/thread/444708"&gt;this&lt;/A&gt; post as it can guide you through the changes needed to use the USB-KW41Z to develop your applications.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt; Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 16:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-KW41Z-Demo-gpio-led-output-wont-seem-to-work/m-p/874752#M52037</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-03-07T16:20:41Z</dc:date>
    </item>
  </channel>
</rss>