<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK82: SB key programming</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-SB-key-programming/m-p/874042#M52002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not able to find FlashProgramOnce in latest SDK 2.5.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;8.6 SB File Decryption Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SB key&lt;BR /&gt;begins at offset 0x30 in the program once registers.&lt;BR /&gt;For example, to program a key of 000102030405060708090A0B0C0D0E0F:&lt;BR /&gt;• FlashProgramOnce to index 0x30 with 4 bytes of 0x03020100&lt;BR /&gt;• FlashProgramOnce to index 0x31 with 4 bytes of 0x07060504&lt;BR /&gt;• FlashProgramOnce to index 0x32 with 4 bytes of 0x0B0A0908&lt;BR /&gt;• FlashProgramOnce to index 0x33 with 4 bytes of 0x0F0E0D0C&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is current equivalent of this function what can be used for write SB key to K82 MCU and SDK 2.5x ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Apr 2019 12:42:33 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2019-04-02T12:42:33Z</dc:date>
    <item>
      <title>K82: SB key programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-SB-key-programming/m-p/874042#M52002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not able to find FlashProgramOnce in latest SDK 2.5.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;8.6 SB File Decryption Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SB key&lt;BR /&gt;begins at offset 0x30 in the program once registers.&lt;BR /&gt;For example, to program a key of 000102030405060708090A0B0C0D0E0F:&lt;BR /&gt;• FlashProgramOnce to index 0x30 with 4 bytes of 0x03020100&lt;BR /&gt;• FlashProgramOnce to index 0x31 with 4 bytes of 0x07060504&lt;BR /&gt;• FlashProgramOnce to index 0x32 with 4 bytes of 0x0B0A0908&lt;BR /&gt;• FlashProgramOnce to index 0x33 with 4 bytes of 0x0F0E0D0C&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is current equivalent of this function what can be used for write SB key to K82 MCU and SDK 2.5x ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2019 12:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-SB-key-programming/m-p/874042#M52002</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-04-02T12:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: K82: SB key programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-SB-key-programming/m-p/874043#M52003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please check &lt;STRONG&gt;FTFx_CMD_ProgramOnce()&lt;/STRONG&gt; function located in&lt;STRONG&gt; fsl_ftfx_controller.c&lt;/STRONG&gt; driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 22:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-SB-key-programming/m-p/874043#M52003</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-04-03T22:59:16Z</dc:date>
    </item>
  </channel>
</rss>