<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KM Family's NMI pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM-Family-s-NMI-pin/m-p/872974#M51951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;This is the way of how NMI_b working. When NMI_EN=1, NMI_b pin is enabled. When it is 0, NMI_b pin is disabled. Whatever mode you set, NMI_b should connect a pull-up resistor. If you pull down it, you'll meet many trouble.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 06:52:42 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-03-21T06:52:42Z</dc:date>
    <item>
      <title>KM Family's NMI pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM-Family-s-NMI-pin/m-p/872973#M51950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am always indebted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the KM Family's MKM14Z64A.&lt;/P&gt;&lt;P&gt;I have a question about the NMI pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm switching after reset to use the NMI pin for GPIO.&lt;BR /&gt;Also, because we want to disable NMI, we are programming the Flash Option Register NMI_EN = 0.&lt;/P&gt;&lt;P&gt;If the CPU is mounted on a board with this pin pulled down due to hardware reasons and the flash loader is transferred to RAM and executed, it will fail.&lt;/P&gt;&lt;P&gt;After executing all erase commands from the initial state CPU or CMSIS-DAP, it will jump to the NMI vector and runaway.&lt;/P&gt;&lt;P&gt;Moreover, at this time, since the secure bit is also on the secure side immediately after the entire erase, even access is not possible.&lt;/P&gt;&lt;P&gt;Is there any way to write successfully with the NMI pin pulled down?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my opinion, NMI_EN of Flash Option Register is 0 if NMI is enabled and 1 is prohibited.&lt;/P&gt;&lt;P&gt;Thank you for your instruction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 04:28:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM-Family-s-NMI-pin/m-p/872973#M51950</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-03-20T04:28:27Z</dc:date>
    </item>
    <item>
      <title>Re: KM Family's NMI pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM-Family-s-NMI-pin/m-p/872974#M51951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi jun,&lt;/P&gt;&lt;P&gt;This is the way of how NMI_b working. When NMI_EN=1, NMI_b pin is enabled. When it is 0, NMI_b pin is disabled. Whatever mode you set, NMI_b should connect a pull-up resistor. If you pull down it, you'll meet many trouble.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 06:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM-Family-s-NMI-pin/m-p/872974#M51951</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-03-21T06:52:42Z</dc:date>
    </item>
  </channel>
</rss>