<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: produce a simple PWM signal usingand glow the RGB LED</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/produce-a-simple-PWM-signal-usingand-glow-the-RGB-LED/m-p/872688#M51947</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="337978" data-username="srirammarisetty_9" href="https://community.nxp.com/people/srirammarisetty_9"&gt;sriram marisetty&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please refer to the FRDM-K22 sdk code, the official FTM code already&amp;nbsp; connect the FTM PWM pin to the RGB LED.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can download the code from this link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Then refer to this code:&lt;/P&gt;&lt;P&gt;SDK_2.5.0_FRDM-K22F\boards\frdmk22f\driver_examples\ftm\simple_pwm\iar&lt;/P&gt;&lt;P&gt;The PWM pin is PTA1, it is FTM0_CH6, it connect to RED_LED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2019 09:40:27 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2019-03-20T09:40:27Z</dc:date>
    <item>
      <title>produce a simple PWM signal usingand glow the RGB LED</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/produce-a-simple-PWM-signal-usingand-glow-the-RGB-LED/m-p/872687#M51946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i need to produce a simple PWM signal using FTM and I need to glow the RGB LED when the PWM is high and turn the LED off when it is low. so, I generated the PWM but I am unable to sinc t with the RGB LED. can you please help me.I need to do this as soon as possible and I am using freedom k22 board. Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 03:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/produce-a-simple-PWM-signal-usingand-glow-the-RGB-LED/m-p/872687#M51946</guid>
      <dc:creator>srirammarisetty</dc:creator>
      <dc:date>2019-03-20T03:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: produce a simple PWM signal usingand glow the RGB LED</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/produce-a-simple-PWM-signal-usingand-glow-the-RGB-LED/m-p/872688#M51947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="337978" data-username="srirammarisetty_9" href="https://community.nxp.com/people/srirammarisetty_9"&gt;sriram marisetty&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please refer to the FRDM-K22 sdk code, the official FTM code already&amp;nbsp; connect the FTM PWM pin to the RGB LED.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can download the code from this link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Then refer to this code:&lt;/P&gt;&lt;P&gt;SDK_2.5.0_FRDM-K22F\boards\frdmk22f\driver_examples\ftm\simple_pwm\iar&lt;/P&gt;&lt;P&gt;The PWM pin is PTA1, it is FTM0_CH6, it connect to RED_LED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 09:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/produce-a-simple-PWM-signal-usingand-glow-the-RGB-LED/m-p/872688#M51947</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-03-20T09:40:27Z</dc:date>
    </item>
  </channel>
</rss>