<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックI cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870478#M51855</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just downloaded the MCUXpresso&amp;nbsp;10.3.1 build 2233 (32-bit) for the first time to use with my new FRDM-KW41Z board and I have hit a snag when I try to debug any program in that it says it cannot link any probe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it is a case of me trying to run before crawling without knowing what I was doing so I am guessing I have messed up some settings along the way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow, I have worked out that the&amp;nbsp;&lt;SPAN&gt;FRDM-KW41Z board uses the SEGGER J-Link USB drivers (the clue I eventually stumbled upon was in the device flash folder where there is an html that redirects to SEGGER).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I then found the SEGGER folder on my Windows 10 computer and prior to stumbling upon the&amp;nbsp;JLinkConfig program I even downloaded another version of SEGGER, so now I have two versions 6.4.2 and 6.4.4. When using the&amp;nbsp;JLinkConfig.exe application (using either SEGGER version) it would find my board and it shows the serial number etc. and can confirm that firmware is ok.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So it would seem that the board and openSDA driver looks ok to me.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Back to MCUXpresso. So if I click on Debug option or click on it when holding shift key to force it to "probe rediscovery" I end up at the same place. A dialogue box opens for probes discovered with the message "No compatible probes available." The IDE console also has a message "No probes found". Now at some stage during the "let me try this stab-in-the-dark" approach I would sometimes get an option to choose a SEGGER file. Either I got the right file choice or not, as this option no longer pops up.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I then discovered a "Debug Config" option. Here I tried clicking on the "GDB SEGGER Interface Debugging" option to create a new launch configuration. Then clicking on the "debugging" tab it gave me a bunch of config options. But here when clicking on the "Device" drop-down menu the KW41Z board is not listed. So I could not proceed any further.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am now at a complete loss as to what to do next. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am also rather curious to know how does one change the SEGGER version for example as cannot see in the IDE how this is linked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Anyhow, any advice and assistance will be greatly appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Mar 2019 21:32:51 GMT</pubDate>
    <dc:creator>gerrikoio</dc:creator>
    <dc:date>2019-03-19T21:32:51Z</dc:date>
    <item>
      <title>I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870478#M51855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just downloaded the MCUXpresso&amp;nbsp;10.3.1 build 2233 (32-bit) for the first time to use with my new FRDM-KW41Z board and I have hit a snag when I try to debug any program in that it says it cannot link any probe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it is a case of me trying to run before crawling without knowing what I was doing so I am guessing I have messed up some settings along the way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow, I have worked out that the&amp;nbsp;&lt;SPAN&gt;FRDM-KW41Z board uses the SEGGER J-Link USB drivers (the clue I eventually stumbled upon was in the device flash folder where there is an html that redirects to SEGGER).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I then found the SEGGER folder on my Windows 10 computer and prior to stumbling upon the&amp;nbsp;JLinkConfig program I even downloaded another version of SEGGER, so now I have two versions 6.4.2 and 6.4.4. When using the&amp;nbsp;JLinkConfig.exe application (using either SEGGER version) it would find my board and it shows the serial number etc. and can confirm that firmware is ok.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So it would seem that the board and openSDA driver looks ok to me.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Back to MCUXpresso. So if I click on Debug option or click on it when holding shift key to force it to "probe rediscovery" I end up at the same place. A dialogue box opens for probes discovered with the message "No compatible probes available." The IDE console also has a message "No probes found". Now at some stage during the "let me try this stab-in-the-dark" approach I would sometimes get an option to choose a SEGGER file. Either I got the right file choice or not, as this option no longer pops up.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I then discovered a "Debug Config" option. Here I tried clicking on the "GDB SEGGER Interface Debugging" option to create a new launch configuration. Then clicking on the "debugging" tab it gave me a bunch of config options. But here when clicking on the "Device" drop-down menu the KW41Z board is not listed. So I could not proceed any further.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am now at a complete loss as to what to do next. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am also rather curious to know how does one change the SEGGER version for example as cannot see in the IDE how this is linked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Anyhow, any advice and assistance will be greatly appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 21:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870478#M51855</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2019-03-19T21:32:51Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870479#M51856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Further to my debug problem, I have subsequently discovered that the&amp;nbsp;KW41Z board is in the device list and is listed as MKW41Z...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that with the search algorithm used you have to get the first letter correct otherwise it does not find any matching terms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I select my board from the device list and then attempt to debug, the debug session then comes up with a new error message "The launch configuration '---program name---' is incompatible with this version of&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;MCUXpresso&amp;nbsp;IDE"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 16:40:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870479#M51856</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2019-03-21T16:40:35Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870480#M51857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I completed a reinstall of MCUXpresso IDE v10.3.1 [Build 2233] [2019-02-20] and was able to recreate the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first time I try and debug the FRDM-KW41Z board I get this message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73706iD899F52EE2B2A549/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I then had to manually find where the SEGGER directory is on my PC and I selected this file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Program Files\SEGGER\JLink_V642b\JLinkGDBServerCL.exe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Maybe someone can confirm if this is the correct selection here.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also found out where I can change this option, should I need to change it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73715i5781772B67CF3297/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 22:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870480#M51857</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2019-03-21T22:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870481#M51858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, with a bit of trial and error I figured this one out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The first thing I had to do was browse and select the "JLinkRegistration.exe" file for the "J-Link Server executable" then "Apply and Close".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then when I choose DEBUG it throws up a SEGGER registration screen. I filled in the details etc. and sent these off.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I return to Windows preference options and now choose the&amp;nbsp;"JLinkGDBServerCL.exe" file and "Apply and Close"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I choose DEBUG&amp;nbsp;it finds the serial number and I enter the debug session.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, there you go. Who would have thought?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At least I'm now up to speed on MCUXpresso's JLink options now...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 22:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870481#M51858</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2019-03-21T22:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870482#M51859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Hi Colin&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Did you look at some of &lt;/SPAN&gt;the training&lt;SPAN style="font-size: 15px;"&gt; that we provide?&lt;/SPAN&gt;&lt;/P&gt;&lt;H1&gt;&lt;SPAN style="font-size: 15px;"&gt;&lt;A href="https://www.nxp.com/video/mcuxpresso-ide-importing-sdk-example-project:MCUXPRESSO-IDE-IMPORTING-SDK-EX"&gt;MCUXpresso IDE - Importing SDK Example Project&lt;/A&gt;&lt;/SPAN&gt;&lt;/H1&gt;&lt;H1&gt;&lt;SPAN style="font-size: 15px;"&gt;&lt;A href="https://www.nxp.com/video/mcuxpresso-ide-project-settings:MCUXPRESSO-IDE-PROJECT-SETTINGS"&gt;MCUXpresso IDE - Project Settings&lt;/A&gt;&lt;/SPAN&gt;&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;I am not sure if you solved your issue. Please let me know if you have any question&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Mario&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2019 23:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870482#M51859</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-03-22T23:51:05Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870483#M51860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes it is resolved thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also downloaded mcuxpresso on my laptop and had none of these issues. For&lt;/P&gt;&lt;P&gt;some reason the device drivers were not behaving properly on my desktop.&lt;/P&gt;&lt;P&gt;But now sorted out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Mar 2019 08:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870483#M51860</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2019-03-23T08:55:49Z</dc:date>
    </item>
    <item>
      <title>Re: I cannot debug my FRDM-KW41Z as MCUXpresso cannot link to probes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870484#M51861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For anyone else who has this problem and comes across this post, I had the same problem and the solution that worked for me was very different but worth trying.&amp;nbsp; Make sure you have the "main" source file for the project opened in the editor.&amp;nbsp; Nothing I did would let me select the debug option until I did this.&amp;nbsp; As soon as I opened the file, everything worked magically...&lt;/P&gt;&lt;P&gt;-Will&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 13:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-cannot-debug-my-FRDM-KW41Z-as-MCUXpresso-cannot-link-to-probes/m-p/870484#M51861</guid>
      <dc:creator>william_lyons</dc:creator>
      <dc:date>2019-12-04T13:55:43Z</dc:date>
    </item>
  </channel>
</rss>