<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Low Voltage Warning interrupt doesn't trigger at configured trip point. Kinetis MK02FN128VFM10. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870353#M51846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the suggested code in the link you sent didn’t actually change the behavior, it did trigger a thought about how I was using the LVD/LVW control registers.&lt;/P&gt;&lt;P&gt;I had the LVD set to the low voltage trip - &lt;STRONG&gt;low&lt;/STRONG&gt; range, but intended to use the low voltage trip – &lt;STRONG&gt;high&lt;/STRONG&gt; range for the LVW.&lt;/P&gt;&lt;P&gt;I reconfigured LVD to use the high trip range, and it is now working as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 18:38:54 GMT</pubDate>
    <dc:creator>matthewking</dc:creator>
    <dc:date>2019-03-21T18:38:54Z</dc:date>
    <item>
      <title>Low Voltage Warning interrupt doesn't trigger at configured trip point. Kinetis MK02FN128VFM10.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870351#M51844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the LVW interrupt in register PMC_LVDSC2 to quickly identify brown-out/power down scenarios.&lt;/P&gt;&lt;P&gt;I am using the "Low-voltage warning thresholds — high range", and have tried each of the 4 possible trip points within the high range: 2.7V, 2.8V, 2.9V, 2.3V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The microcontroller does detect the low voltage event, but always at 2.38V (+/- .02V), regardless of the configured trip point. I know this because I toggle an I/O pin when the ISR fires, and I see the supply voltage to the MCU at the time the I/O toggles.&lt;/P&gt;&lt;P&gt;Is there a known errata on the LVW interrupt trip point voltage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 15:52:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870351#M51844</guid>
      <dc:creator>matthewking</dc:creator>
      <dc:date>2019-03-19T15:52:44Z</dc:date>
    </item>
    <item>
      <title>Re: Low Voltage Warning interrupt doesn't trigger at configured trip point. Kinetis MK02FN128VFM10.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870352#M51845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Matthew King,&lt;/P&gt;&lt;P&gt;I didn't find related errata in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/errata/KINETIS_K_0N36M.pdf" shape="rect" target="_blank"&gt;KINETIS_K_0N36M&lt;/A&gt;.&lt;BR clear="none" /&gt;Please refer the answer in:&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/451480" shape="rect" target="_blank"&gt;mk60dn512 low voltage warning&lt;/A&gt;&lt;BR clear="none" /&gt;Would you please modify the codes and test it on your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 08:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870352#M51845</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-03-21T08:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: Low Voltage Warning interrupt doesn't trigger at configured trip point. Kinetis MK02FN128VFM10.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870353#M51846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While the suggested code in the link you sent didn’t actually change the behavior, it did trigger a thought about how I was using the LVD/LVW control registers.&lt;/P&gt;&lt;P&gt;I had the LVD set to the low voltage trip - &lt;STRONG&gt;low&lt;/STRONG&gt; range, but intended to use the low voltage trip – &lt;STRONG&gt;high&lt;/STRONG&gt; range for the LVW.&lt;/P&gt;&lt;P&gt;I reconfigured LVD to use the high trip range, and it is now working as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 18:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-Voltage-Warning-interrupt-doesn-t-trigger-at-configured-trip/m-p/870353#M51846</guid>
      <dc:creator>matthewking</dc:creator>
      <dc:date>2019-03-21T18:38:54Z</dc:date>
    </item>
  </channel>
</rss>