<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MKM34Z256 Comparator input impedance</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870178#M51837</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Colleagues,&lt;/P&gt;&lt;P&gt;our customer wants to use MKM34 comparators in their application&amp;nbsp; And there is question they didn’t find the answer in the documents:&lt;/P&gt;&lt;P&gt;They want to use the three high speed comparator modules in the KM34Z256 to detect an overcurrent as fast as possible. (one for each phase).&amp;nbsp;To connect our external circuit to the comparator input, they must know their input impedance. If the impedance of the comparator inputs is as low as the ADC inputs (some kOhm) than they must add separate impedance converter.&lt;BR /&gt;If the input is like a CMOS-Comparator (several MOhm) then the impedance converters are not needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can you tell me the input impedance of the comparator inputs?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and kind regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Mar 2019 10:48:52 GMT</pubDate>
    <dc:creator>petr_uhlir</dc:creator>
    <dc:date>2019-03-19T10:48:52Z</dc:date>
    <item>
      <title>MKM34Z256 Comparator input impedance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870178#M51837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Colleagues,&lt;/P&gt;&lt;P&gt;our customer wants to use MKM34 comparators in their application&amp;nbsp; And there is question they didn’t find the answer in the documents:&lt;/P&gt;&lt;P&gt;They want to use the three high speed comparator modules in the KM34Z256 to detect an overcurrent as fast as possible. (one for each phase).&amp;nbsp;To connect our external circuit to the comparator input, they must know their input impedance. If the impedance of the comparator inputs is as low as the ADC inputs (some kOhm) than they must add separate impedance converter.&lt;BR /&gt;If the input is like a CMOS-Comparator (several MOhm) then the impedance converters are not needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can you tell me the input impedance of the comparator inputs?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and kind regards,&lt;/P&gt;&lt;P&gt;Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 10:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870178#M51837</guid>
      <dc:creator>petr_uhlir</dc:creator>
      <dc:date>2019-03-19T10:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: ABB: MKM34Z256 Comparator input impedance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870179#M51838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just asked the design team about this parameter. I will let you know as soon as I have any update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 22:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870179#M51838</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-03-20T22:04:29Z</dc:date>
    </item>
    <item>
      <title>Re: ABB: MKM34Z256 Comparator input impedance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870180#M51839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I received information from the design team:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The answer is impedance &amp;lt;5K ohm after checking with IP owner.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 15:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34Z256-Comparator-input-impedance/m-p/870180#M51839</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-03-21T15:46:08Z</dc:date>
    </item>
  </channel>
</rss>