<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K82 : optimal clock tree in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868759#M51809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene Hiihtaja,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to use internal IRC48M, you can use the IRC48Mhz as the PLL input ,then configure it like this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78008i5A400665158C4397/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You also can use the MCUxpresso Config Tool to configure it.&lt;/P&gt;&lt;P&gt;But about the low power consumption, if you work with 120Mhz, the power consumption won't be very low, unless you enter the low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 08:27:13 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2019-01-11T08:27:13Z</dc:date>
    <item>
      <title>K82 : optimal clock tree</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868758#M51808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to create optimal clock tree for my configuration. I think by using it I can have less power consumption&lt;/P&gt;&lt;P&gt;in RUN mode and LLS mode. And have fast wakeup from LLS3 to RUN by using external/internal LLWU as wakeup source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have both crystal oscillators and use couple I2C ( mastrer and slave), RTC, WDOG and LPUART for debug terminal.&lt;/P&gt;&lt;P&gt;LTC and TRNG in use as well. LPO is need for LLWU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see from DS that IRC48 if used consume something and better to avoid usage of it.&lt;/P&gt;&lt;P&gt;I need core/system clock 120 Mhz and Bus clock 60 Mhz.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But MCG might have different configuration.&lt;/P&gt;&lt;P&gt;LPUART can take clock from crystal oscillator directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be overall clocking scheme recommendations what lead to lower power consumption and fast wakeup&lt;/P&gt;&lt;P&gt;from LLS3 by using LLWU ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 13:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868758#M51808</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-01-10T13:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : optimal clock tree</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868759#M51809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene Hiihtaja,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to use internal IRC48M, you can use the IRC48Mhz as the PLL input ,then configure it like this :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78008i5A400665158C4397/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You also can use the MCUxpresso Config Tool to configure it.&lt;/P&gt;&lt;P&gt;But about the low power consumption, if you work with 120Mhz, the power consumption won't be very low, unless you enter the low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 08:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868759#M51809</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-01-11T08:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : optimal clock tree</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868760#M51810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes I'm using&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MCUxpresso Config Tool as initial configurator for my project.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MCU wakeup to 120Mhz quite rare and other time stay in LLS3 mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;But in documentation mentioned that wakeup time is depends from clock configuration due stabilisation time for some clock units.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;And I also believe that minimal path in clocking tree should bring some saving.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;In LLS3 mode , proper GPIO pin configuration for all unused pin might have major effect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Eugene&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 08:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-optimal-clock-tree/m-p/868760#M51810</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-01-11T08:33:53Z</dc:date>
    </item>
  </channel>
</rss>