<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK22FN1M0A, FlexRAM, and EEPROM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FN1M0A-FlexRAM-and-EEPROM/m-p/867956#M51779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MK22FN&amp;nbsp; does NOT have EEPROM functionality. FX has. Could you double check it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1). High endurance EEPROM is compare to the traditional EEPROM. Writing the parameters can wear out the EEPROM, since it is only guaranteed to about 100K erase/write cycles.&amp;nbsp;&amp;nbsp; High endurance means comparably greater erase/write cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2).Yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3). Since K22FN has no EEPROM,&amp;nbsp; there is no&amp;nbsp; SDK examples to using the EERPOM feature in this package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 08:08:30 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-03-21T08:08:30Z</dc:date>
    <item>
      <title>MK22FN1M0A, FlexRAM, and EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FN1M0A-FlexRAM-and-EEPROM/m-p/867955#M51778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using an MK22FN1M0A. When I read from register SIM_FCFG1, it reports that 4K of EEPROM is available, but 0K of NVRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the reference manual, K22P144M120SF5V2RM.pdf, specifies that the MK22FN1M0A, in chapter&amp;nbsp;2.3, Orderable Parts, does not have EEPROM. It does have 4K of FlexRAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand to access EEPROM&amp;nbsp;on the Kinetis series, one must have FlexNVM available, but FlexRAM can be used as high-endurance EEPROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1- What is 'high-endurance EEPROM'?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2-Am I correct that Data Flash IFR 0x03FD:EESIZE specifies how much FlexRAM is used as EEPROM? [29.3.3.1]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3-Are there any SDK examples on configuring and using the EEPROM feature of FlexRAM?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2019 14:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FN1M0A-FlexRAM-and-EEPROM/m-p/867955#M51778</guid>
      <dc:creator>Keith4DSmith</dc:creator>
      <dc:date>2019-03-18T14:45:15Z</dc:date>
    </item>
    <item>
      <title>Re: MK22FN1M0A, FlexRAM, and EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FN1M0A-FlexRAM-and-EEPROM/m-p/867956#M51779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MK22FN&amp;nbsp; does NOT have EEPROM functionality. FX has. Could you double check it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1). High endurance EEPROM is compare to the traditional EEPROM. Writing the parameters can wear out the EEPROM, since it is only guaranteed to about 100K erase/write cycles.&amp;nbsp;&amp;nbsp; High endurance means comparably greater erase/write cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2).Yes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3). Since K22FN has no EEPROM,&amp;nbsp; there is no&amp;nbsp; SDK examples to using the EERPOM feature in this package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 08:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22FN1M0A-FlexRAM-and-EEPROM/m-p/867956#M51779</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-03-21T08:08:30Z</dc:date>
    </item>
  </channel>
</rss>