<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKL82Z - JLink doesn't work in STOP mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864222#M51687</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For measuring low-power current draw, I programmed an application into KL82Z flash that immediately puts the device into STOP, via POWER_SYS_SetMode().&amp;nbsp; However, now I can't re-program or erase it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JLink fails to connect with the attached errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also tried booting the KL82Z into ROM bootloader and running `blhost`, but that doesn't seem to work either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this expected?&amp;nbsp; Is there any other way to recover the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using KSDK 1.3.0 for KL82Z, and have a JLink Base.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Feb 2019 14:48:49 GMT</pubDate>
    <dc:creator>nickbedbury</dc:creator>
    <dc:date>2019-02-14T14:48:49Z</dc:date>
    <item>
      <title>KL82Z - JLink doesn't work in STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864222#M51687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For measuring low-power current draw, I programmed an application into KL82Z flash that immediately puts the device into STOP, via POWER_SYS_SetMode().&amp;nbsp; However, now I can't re-program or erase it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JLink fails to connect with the attached errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also tried booting the KL82Z into ROM bootloader and running `blhost`, but that doesn't seem to work either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this expected?&amp;nbsp; Is there any other way to recover the device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using KSDK 1.3.0 for KL82Z, and have a JLink Base.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 14:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864222#M51687</guid>
      <dc:creator>nickbedbury</dc:creator>
      <dc:date>2019-02-14T14:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: KL82Z - JLink doesn't work in STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864223#M51688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well...that was easy.&amp;nbsp; It seems I didn't put it into ROM bootloader properly like I thought.&amp;nbsp; After checking that, `blhost` works fine to erase it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 14:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864223#M51688</guid>
      <dc:creator>nickbedbury</dc:creator>
      <dc:date>2019-02-14T14:53:23Z</dc:date>
    </item>
    <item>
      <title>Re: KL82Z - JLink doesn't work in STOP mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864224#M51689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick Bedbury,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your solutions sharing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you meet the other question in the future, welcome to create the new question post and let us know.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 11:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82Z-JLink-doesn-t-work-in-STOP-mode/m-p/864224#M51689</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-02-15T11:42:30Z</dc:date>
    </item>
  </channel>
</rss>