<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K82 : GPIO lines active and passive filters in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864145#M51686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So If clock filter from LPO and some GPIO should detect ( and LLWU wakeup as well)&amp;nbsp; LowState &amp;gt; 50 ms ( filterWidth = 50 ) I can use it ?&lt;/P&gt;&lt;P&gt;One port can have one filter but each pin can be enabled to have this filter individually ?&lt;/P&gt;&lt;P&gt;Or this filter is more to filter falling and rising edges and can't be used for levels ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2019 12:04:54 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2019-01-24T12:04:54Z</dc:date>
    <item>
      <title>K82 : GPIO lines active and passive filters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864143#M51684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain about GPIO lines passive and digital filters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can the same pin have enabled passive and digital filter at the same time ?&lt;/P&gt;&lt;P&gt;Or really it dosn't have sense ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in RM like this :&lt;/P&gt;&lt;P&gt;"The filter width in clock size is the same for all enabled digital filters within one port and&lt;BR /&gt;must be changed only when all digital filters for that port are disabled.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Does it means that different gpio lines in one port can't have different digital pin configurations ?&lt;/P&gt;&lt;P&gt;It can be enabled/disabled but id enabled it is the same for all port's pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 09:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864143#M51684</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-01-09T09:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : GPIO lines active and passive filters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864144#M51685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Passive filter is a analog low pass filter (10 MHz to 30 MHz bandwidth).&lt;BR /&gt;Passive filter deals with analog signals and using to filter high frequency noise, the frequency more than 30MHz signal will be filtered.&lt;BR /&gt;Passive filter frequency is fixed and could not be modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Digital filter deals with digital input signals. Digital filter sets a filter gate (filter width in clock size), if input signal shorter than setting filter width, the input signal will be filtered.&lt;BR /&gt;The digital filter gate could be set by filter registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 02:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864144#M51685</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-01-24T02:33:25Z</dc:date>
    </item>
    <item>
      <title>Re: K82 : GPIO lines active and passive filters</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864145#M51686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So If clock filter from LPO and some GPIO should detect ( and LLWU wakeup as well)&amp;nbsp; LowState &amp;gt; 50 ms ( filterWidth = 50 ) I can use it ?&lt;/P&gt;&lt;P&gt;One port can have one filter but each pin can be enabled to have this filter individually ?&lt;/P&gt;&lt;P&gt;Or this filter is more to filter falling and rising edges and can't be used for levels ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 12:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K82-GPIO-lines-active-and-passive-filters/m-p/864145#M51686</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2019-01-24T12:04:54Z</dc:date>
    </item>
  </channel>
</rss>