<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis bootloader start from application in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864127#M51674</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See the attached files for correctly formatted code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.h:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;void boot_loader_start( void ) __attribute__ ((noreturn));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.c:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* Function Pointer returning void, passed void pointer: */&lt;BR /&gt;void (*_boot_loader_start)( void * arg );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void boot_loader_start( void )&lt;BR /&gt;{&lt;BR /&gt; /* Read the function address from the ROM API tree: */&lt;BR /&gt; uint32_t const _boot_loader_start_address = **(uint32_t **)(0x1C00001CUL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Turn address in to a function pointer: */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; _boot_loader_start = (void (*)(void * arg))_boot_loader_start_address;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;_boot_loader_start( NULL ); /* Call the function. Will not return from here */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for(;;) /* Pacify the compiler about returning from a no return function */&lt;BR /&gt; ;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Mar 2019 18:07:57 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2019-03-04T18:07:57Z</dc:date>
    <item>
      <title>Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864126#M51673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to initiate firmware upgrade from application, so I want to start bootloader (KBOOT 2) from application and keep it running. I didn't find this option in bootloader. Do I have to program it myself? Can you recommend how to do it? Eg. write some register that is guaranted not to change during reset with an information, that bootloader should and perform software reset to enter bootloader...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next question: I would like to enter my app with all peripherals, clocks, etc. unitialized. I think Kinetis bootloader initializes some peripherals, clocks, etc. and then it jumps to application's reset vector. Is there an option, where e.g. bootloader writes some register that is&amp;nbsp;guaranted not to change during reset with an information that application should run, then it executes software reset and during next bootloader startup, it checks that register and it immediatelly jumps to the application? Or, again, do I have to implement it myself?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Mar 2019 16:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864126#M51673</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-03T16:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864127#M51674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See the attached files for correctly formatted code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.h:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;void boot_loader_start( void ) __attribute__ ((noreturn));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.c:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* Function Pointer returning void, passed void pointer: */&lt;BR /&gt;void (*_boot_loader_start)( void * arg );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void boot_loader_start( void )&lt;BR /&gt;{&lt;BR /&gt; /* Read the function address from the ROM API tree: */&lt;BR /&gt; uint32_t const _boot_loader_start_address = **(uint32_t **)(0x1C00001CUL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Turn address in to a function pointer: */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; _boot_loader_start = (void (*)(void * arg))_boot_loader_start_address;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;_boot_loader_start( NULL ); /* Call the function. Will not return from here */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for(;;) /* Pacify the compiler about returning from a no return function */&lt;BR /&gt; ;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 18:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864127#M51674</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2019-03-04T18:07:57Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864128#M51675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. I don't use ROM bootloader but flash resident bootloader. I guess I haveto change the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;0x1C00001CUL to my bootloader's start address which is 0x0 as my bootloader is at the beginning of the flash. So I guess this code can be replaced by performing software cpu reset.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The problem is: when bootloader starts, it detects valid application and immediatelly jumps back to my application. I want the bootloader to run and wait till host (USB HID in my case) connects to it and performs firmware upgrade.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 18:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864128#M51675</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-04T18:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864129#M51676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I want to start bootloader (KBOOT 2)&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I took that as you were using the KBOOT-2 bootloader in the standard ROM.&lt;BR /&gt;The ROM gives the address of the actual bootloader start at a known location, so have to look up that value before using it.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 21:29:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864129#M51676</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2019-03-04T21:29:06Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864130#M51677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But still, will the bootloader wait for the user to connect to it or will it detect valid application and automatically jump to it? I think this is not solution to my problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 06:57:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864130#M51677</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-05T06:57:55Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864131#M51678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;Flashloader hasn't run_bootloader() function. But in fact, if you look into its final code bootloader_user_entry(), it only reset the chip. So, if you want to jump back to bootloader, just call NVIC_SystemReset().&lt;/P&gt;&lt;P&gt;After reset, the bootloader will wait for peripheral connection. The default time is 5000ms which is defined in bootloader_config.h. The macro name is BL_DEFAULT_PERIPHERAL_DETECT_TIMEOUT.&lt;/P&gt;&lt;P&gt;If you want to keep some value when system reset, you can put the value in sytem register file. It reset by POR only. Not all of kinetis device has this register file. But most of them have. If the chip you're using hasn't it, you have to save data into flash or external memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 03:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864131#M51678</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-03-06T03:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864132#M51679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing,&lt;/P&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In normal situation the bootloader should not wait and should jump to valid application immediatelly (the user of my device can't wait 5 seconds every time the device is turned on for bootloader to timeout and jump to application).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In a situation, where user of my application explicitly requests bootloader to run, the bootloader should wait 5 s (or even longer, till next reset) for peripheral to connect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is that possible with kinetis bootloader?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 08:23:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864132#M51679</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-06T08:23:13Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864133#M51680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, you have to modify the code. But if the MCU has register file, I think it's not very difficult.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 09:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864133#M51680</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-03-07T09:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864134#M51681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No problem, I will modify it. When switching between bootloader and application I prefere performing that by writing some register/RAM with information whether bootloader/app should run followed by software reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is RAM or some registers guaranteed not to be modified during software reset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not I thought about using some RTC registers (e.g. RTC alaram register which I'm not going to use in my app) which are persistent as long as VBAT is present.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 09:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864134#M51681</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-07T09:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864135#M51682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;please search "register file" in reference manual.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67117iC3998F32A0AA41C3/image-size/large?v=v2&amp;amp;px=999" title="registerfile.png" alt="registerfile.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 02:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864135#M51682</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-03-08T02:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis bootloader start from application</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864136#M51683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry, I didn't&amp;nbsp;understand what you mean by register file in your previous post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So great, there will be no problem in implementing what I want. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 13:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-bootloader-start-from-application/m-p/864136#M51683</guid>
      <dc:creator>dusek_martin</dc:creator>
      <dc:date>2019-03-08T13:50:30Z</dc:date>
    </item>
  </channel>
</rss>