<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: 3bits completely missing on the KV31 FlexBus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/3bits-completely-missing-on-the-KV31-FlexBus/m-p/860383#M51504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, it seems really confused here for the FB_AD.&lt;/P&gt;&lt;P&gt;First, it is stated in the manual that: " FB_AD[23:21] not available on 100-LQFP devices."&lt;/P&gt;&lt;P&gt;And for 64 pin package, the FB_AD only to FB_AD17.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 08:21:13 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2019-02-19T08:21:13Z</dc:date>
    <item>
      <title>3bits completely missing on the KV31 FlexBus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/3bits-completely-missing-on-the-KV31-FlexBus/m-p/860382#M51503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FB_AD21,&amp;nbsp;&lt;SPAN&gt;FB_AD22,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;FB_AD23, are missing in the pin out description for the&amp;nbsp; &lt;SPAN class=""&gt;MKV31F512VL&lt;/SPAN&gt; &lt;BR style="font-weight: normal;" /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Where did they go?&amp;nbsp;FB_AD31:FB_AD24 and&amp;nbsp;FB_AD20:FB_AD00 are all identified in the specification.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These three(3) bits are also missing from the config tool, yet the write-up for the FlexBus clearly calls for all 32 bits to be available.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 21:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/3bits-completely-missing-on-the-KV31-FlexBus/m-p/860382#M51503</guid>
      <dc:creator>michaelbanak</dc:creator>
      <dc:date>2019-02-13T21:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: 3bits completely missing on the KV31 FlexBus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/3bits-completely-missing-on-the-KV31-FlexBus/m-p/860383#M51504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, it seems really confused here for the FB_AD.&lt;/P&gt;&lt;P&gt;First, it is stated in the manual that: " FB_AD[23:21] not available on 100-LQFP devices."&lt;/P&gt;&lt;P&gt;And for 64 pin package, the FB_AD only to FB_AD17.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 08:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/3bits-completely-missing-on-the-KV31-FlexBus/m-p/860383#M51504</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-19T08:21:13Z</dc:date>
    </item>
  </channel>
</rss>