<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックProgrammed wrong image, is the chip completely dead?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860063#M51462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I made an oops and programmed the wrong image into a Kinetis KE18.&amp;nbsp; Pretty sure the flash configuration field was overwritten with something wrong and I cycled power.&amp;nbsp; Now the BDM can't connect to it to reprogram it.&amp;nbsp; Is there any way to recover, or will the chip have to be replaced?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Feb 2019 13:20:52 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2019-02-13T13:20:52Z</dc:date>
    <item>
      <title>Programmed wrong image, is the chip completely dead?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860063#M51462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I made an oops and programmed the wrong image into a Kinetis KE18.&amp;nbsp; Pretty sure the flash configuration field was overwritten with something wrong and I cycled power.&amp;nbsp; Now the BDM can't connect to it to reprogram it.&amp;nbsp; Is there any way to recover, or will the chip have to be replaced?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 13:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860063#M51462</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2019-02-13T13:20:52Z</dc:date>
    </item>
    <item>
      <title>Re: Programmed wrong image, is the chip completely dead?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860064#M51463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;BDM (Background Debug Mode) =&amp;gt; SWD/JTAG?&lt;/P&gt;&lt;P&gt;If you have turned on 'mass erase disabled' with 'readout protection' (&lt;A class="link-titled" href="https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/" title="https://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/"&gt;How (not) to Secure my Microcontroller | MCU on Eclipse&lt;/A&gt;), then I'm affraid you have to unsolder it as it is really bricked.&lt;/P&gt;&lt;P&gt;If not and if you have a J-Link, you can try to use the approach described in &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/10/05/unlocking-and-erasing-flash-with-segger-j-link/" title="https://mcuoneclipse.com/2014/10/05/unlocking-and-erasing-flash-with-segger-j-link/"&gt;Unlocking and Erasing FLASH with Segger J-Link | MCU on Eclipse&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;If you are using MCUXpresso IDE, it comes with a 'resurrection' tool in the GUI Flash programmer inside the IDE:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72384iA68D57DFBD92C5A8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 13:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860064#M51463</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-02-13T13:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: Programmed wrong image, is the chip completely dead?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860065#M51464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Erich, yes, I have an SWD connection.&amp;nbsp; I have a P&amp;amp;E Multilink for the debugger.&amp;nbsp; Closest thing I have is in the debugger window in MCUXpresso there's a checkbox for "Emergency Kinetis Device Recovery by Full Chip Erase", but it's not responding.&amp;nbsp; I'll see if the newer versions of P&amp;amp;E's flash programmer maybe have an option to try to restore it, but it can't even connect with the version I have.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 13:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programmed-wrong-image-is-the-chip-completely-dead/m-p/860065#M51464</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2019-02-13T13:53:12Z</dc:date>
    </item>
  </channel>
</rss>