<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: what changes do i need to do in flexcan_loopback example from one frdm k64 to another?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-changes-do-i-need-to-do-in-flexcan-loopback-example-from/m-p/858209#M51430</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vimal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a flexcan_interrupt example shows how to use Flexcan driver with 2 boards.&lt;/P&gt;&lt;P&gt;SDK_2.5.0_TWR-K64F120M\boards\twrk64f120m\driver_examples\flexcan\interrupt_transfer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this example, 2 boards are connected through CAN bus. Endpoint A(board A) send a CAN Message to&lt;BR /&gt;Endpoint B(board B) when user press space key in terminal. Endpoint B receive the message, print&lt;BR /&gt;the message content to terminal and echo back the message. Endpoint A will increase the received&lt;BR /&gt;message and waiting for the next transmission of the user initiated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Feb 2019 07:38:52 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-02-13T07:38:52Z</dc:date>
    <item>
      <title>what changes do i need to do in flexcan_loopback example from one frdm k64 to another?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-changes-do-i-need-to-do-in-flexcan-loopback-example-from/m-p/858208#M51429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i'm using 2 frdm k64 kit and im trying to make a CAN communication between two 2 frdm k64 boards.&lt;/P&gt;&lt;P&gt;im using flexcan_loopback example where it sends&amp;nbsp;CAN Message from the Tx Message Buffer to the Rx Message Buffer throuth internal loopback interconnect but i need to send from one board to another board.what changes do i need in this example program to send from one board to another??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 06:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-changes-do-i-need-to-do-in-flexcan-loopback-example-from/m-p/858208#M51429</guid>
      <dc:creator>vimalprasath</dc:creator>
      <dc:date>2019-02-13T06:11:37Z</dc:date>
    </item>
    <item>
      <title>Re: what changes do i need to do in flexcan_loopback example from one frdm k64 to another?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-changes-do-i-need-to-do-in-flexcan-loopback-example-from/m-p/858209#M51430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vimal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a flexcan_interrupt example shows how to use Flexcan driver with 2 boards.&lt;/P&gt;&lt;P&gt;SDK_2.5.0_TWR-K64F120M\boards\twrk64f120m\driver_examples\flexcan\interrupt_transfer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this example, 2 boards are connected through CAN bus. Endpoint A(board A) send a CAN Message to&lt;BR /&gt;Endpoint B(board B) when user press space key in terminal. Endpoint B receive the message, print&lt;BR /&gt;the message content to terminal and echo back the message. Endpoint A will increase the received&lt;BR /&gt;message and waiting for the next transmission of the user initiated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 07:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/what-changes-do-i-need-to-do-in-flexcan-loopback-example-from/m-p/858209#M51430</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-02-13T07:38:52Z</dc:date>
    </item>
  </channel>
</rss>