<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: S9KEA UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEA-UART/m-p/857733#M51415</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ryan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thank you for your interest in NXP kinetis product, I would like to provide service for you.&lt;BR /&gt;Customer is using S9KEAZN64ACLH chip, but I find the code is using the SKEAZ64xxx4, not SKEAZN64xxx2. &lt;BR /&gt;And the according head files is based on the KEA128.&lt;BR /&gt;Actually the KEA128 and the KEAZN64 have a lot of difference.&lt;BR /&gt;I think the hardfault interrupt should enter some area or register which the S9KEAZN64ACLH don't have.&lt;BR /&gt;I don't whether you test the clock or not? eg, bus clock or the system clock, is it correct on your side?&lt;BR /&gt;From your configuration, it should have problems, if you are really using S9KEAZN64ACLH, not the KEAZ64.&lt;BR /&gt;At first, tell you some difference:&lt;BR /&gt;1. KEAZN64 FLL factor is 1024, but KEA128 FLL factor is 1280&lt;BR /&gt;&amp;nbsp;&amp;nbsp; From your code, I find you are using the 1280, SystemCoreClockUpdate function.&lt;BR /&gt;2. KEAZN64 core clock up to 40Mhz, but KEA128 core clock can up to 48Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; KEAZN64 bus clock up to&amp;nbsp; 20Mhz, but KEA128 bus clock can up to 24Mhz.&lt;BR /&gt;3. KEAZN64 internal factory trimmed IRC is 31.25khz, but KEA128 internal IRC is 37.5Khz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; But from your schematic, you are using the external 12Mhz. I don't know why you choose this crystal, 12Mhz is not support.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; If you want to get 40Mhz core clock, it's better to use the 10Mhz, then RDIV=256, then the FLL input clock is 39.0625khz, FLL factor is 1024, 39.0625KHZ*1024=40Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; From your code, I find you configure CLOCK_SETUP=1,&amp;nbsp; and use these code:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; #elif (CLOCK_SETUP == 1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_XTAL_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32768u /* Value of the external crystal or oscillator clock frequency in Hz */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_INT_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32768u&amp;nbsp;&amp;nbsp; /* Value of the internal oscillator clock frequency in Hz&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define DEFAULT_SYSTEM_CLOCK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20971520u /* Default System clock value */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Actually, it is not correct, XTAL clock is not correct, internal clock also not correct.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Please modify it. Even you use the FEI mode, your configuration is not correct. &lt;BR /&gt;&amp;nbsp;&amp;nbsp; You must make sure the clock configuration works OK.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; If you use the FEI mode, the internal IRC is 31.25khz, then 31.25khz*1024= 32Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Then you need to use this core clock and bus clock to configurate your two UART with the correct baudrate.&lt;BR /&gt;&amp;nbsp; This is very important to make the MCU works stably.&lt;BR /&gt;4. Header file, you also can use the SKEAZN64 instead of the KEA128, you can find the header file in the MDK instal path:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; C:\Keil_v5\ARM\PACK\Keil\Kinetis_KEAxx_DFP\1.3.0\Device\Include&lt;BR /&gt;&amp;nbsp;&amp;nbsp; start .s file, you also can use the SKEAZN64, you can find it from :&lt;BR /&gt;&amp;nbsp;&amp;nbsp; C:\Keil_v5\ARM\PACK\Keil\Kinetis_KEAxx_DFP\1.3.0\Device\Source\ARM&lt;BR /&gt;&amp;nbsp;&amp;nbsp; system_xxx.c you can use your own file, but you need to modfy the CPU_XTAL_CLK_HZ, CPU_INT_CLK_HZ,DEFAULT_SYSTEM_CLOCK &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #elif (CLOCK_SETUP == 1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_XTAL_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10000000u /* Value of the external crystal or oscillator clock frequency in Hz if you want to get 40Mhz core clock in FEE mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_INT_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 31250u&amp;nbsp;&amp;nbsp; /* Value of the internal oscillator clock frequency in Hz&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define DEFAULT_SYSTEM_CLOCK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32000000u /* Default System clock value */&lt;BR /&gt;&amp;nbsp; About the DEFAULT_SYSTEM_CLOCK&amp;nbsp; please note, if you BDIV is ICS-&amp;gt;C2 |= (uint8_t)(ICS_C2_BDIV(0x01));, then it should be 32Mhz/2=16Mhz.&lt;BR /&gt;&amp;nbsp; SystemCoreClockUpdate function, modify &lt;BR /&gt;&amp;nbsp; ICSOUTClock *= 1280u;&lt;BR /&gt;&amp;nbsp;to &lt;BR /&gt;&amp;nbsp; ICSOUTClock *= 1024u;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After you modify the header file, .s file and the clock system, then you can test it again.&lt;BR /&gt;If you still have question about the hardfault about uart, I suggest you comment all other code, just leave two UART.&lt;BR /&gt;You can just configure one uart1, then use it as the wake up source, then test it whether it still enter the hardfault or not?&lt;BR /&gt;When you disable the UART0, please clear the accoridng status at first, then disable it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you still have problems after all the above test, please kindly let me know.&lt;BR /&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2019 07:21:52 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2019-01-08T07:21:52Z</dc:date>
    <item>
      <title>S9KEA UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEA-UART/m-p/857732#M51414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt;I&amp;nbsp;am&amp;nbsp;using S9KEAZN64ACLH in E-bicycle, and now facing a uart issue. Please help to check, urgent. thanks! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt;I use both UART0 and UART1, and go to Stop(Deepsleep) mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt; 1. They disable the UART0 then go to __WFI(), when wake the mcu via UAR1 interrupt, it will go to Hardfault interrupt. 2. If they donot disable the UART0, and wake the mcu via UAR1 interrupt, it will wake normally. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt;The simply code and schematic are as attachment, can you help to debug what is the reason of the hardfault? thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #4a4a4d; background-color: #f2f2f5;"&gt; And the IDE is KEIL.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 10:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEA-UART/m-p/857732#M51414</guid>
      <dc:creator>ryanshi</dc:creator>
      <dc:date>2019-01-07T10:40:52Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEA UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEA-UART/m-p/857733#M51415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ryan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thank you for your interest in NXP kinetis product, I would like to provide service for you.&lt;BR /&gt;Customer is using S9KEAZN64ACLH chip, but I find the code is using the SKEAZ64xxx4, not SKEAZN64xxx2. &lt;BR /&gt;And the according head files is based on the KEA128.&lt;BR /&gt;Actually the KEA128 and the KEAZN64 have a lot of difference.&lt;BR /&gt;I think the hardfault interrupt should enter some area or register which the S9KEAZN64ACLH don't have.&lt;BR /&gt;I don't whether you test the clock or not? eg, bus clock or the system clock, is it correct on your side?&lt;BR /&gt;From your configuration, it should have problems, if you are really using S9KEAZN64ACLH, not the KEAZ64.&lt;BR /&gt;At first, tell you some difference:&lt;BR /&gt;1. KEAZN64 FLL factor is 1024, but KEA128 FLL factor is 1280&lt;BR /&gt;&amp;nbsp;&amp;nbsp; From your code, I find you are using the 1280, SystemCoreClockUpdate function.&lt;BR /&gt;2. KEAZN64 core clock up to 40Mhz, but KEA128 core clock can up to 48Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; KEAZN64 bus clock up to&amp;nbsp; 20Mhz, but KEA128 bus clock can up to 24Mhz.&lt;BR /&gt;3. KEAZN64 internal factory trimmed IRC is 31.25khz, but KEA128 internal IRC is 37.5Khz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; But from your schematic, you are using the external 12Mhz. I don't know why you choose this crystal, 12Mhz is not support.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; If you want to get 40Mhz core clock, it's better to use the 10Mhz, then RDIV=256, then the FLL input clock is 39.0625khz, FLL factor is 1024, 39.0625KHZ*1024=40Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; From your code, I find you configure CLOCK_SETUP=1,&amp;nbsp; and use these code:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; #elif (CLOCK_SETUP == 1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_XTAL_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32768u /* Value of the external crystal or oscillator clock frequency in Hz */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_INT_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32768u&amp;nbsp;&amp;nbsp; /* Value of the internal oscillator clock frequency in Hz&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define DEFAULT_SYSTEM_CLOCK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 20971520u /* Default System clock value */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Actually, it is not correct, XTAL clock is not correct, internal clock also not correct.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Please modify it. Even you use the FEI mode, your configuration is not correct. &lt;BR /&gt;&amp;nbsp;&amp;nbsp; You must make sure the clock configuration works OK.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; If you use the FEI mode, the internal IRC is 31.25khz, then 31.25khz*1024= 32Mhz.&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Then you need to use this core clock and bus clock to configurate your two UART with the correct baudrate.&lt;BR /&gt;&amp;nbsp; This is very important to make the MCU works stably.&lt;BR /&gt;4. Header file, you also can use the SKEAZN64 instead of the KEA128, you can find the header file in the MDK instal path:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; C:\Keil_v5\ARM\PACK\Keil\Kinetis_KEAxx_DFP\1.3.0\Device\Include&lt;BR /&gt;&amp;nbsp;&amp;nbsp; start .s file, you also can use the SKEAZN64, you can find it from :&lt;BR /&gt;&amp;nbsp;&amp;nbsp; C:\Keil_v5\ARM\PACK\Keil\Kinetis_KEAxx_DFP\1.3.0\Device\Source\ARM&lt;BR /&gt;&amp;nbsp;&amp;nbsp; system_xxx.c you can use your own file, but you need to modfy the CPU_XTAL_CLK_HZ, CPU_INT_CLK_HZ,DEFAULT_SYSTEM_CLOCK &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #elif (CLOCK_SETUP == 1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_XTAL_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 10000000u /* Value of the external crystal or oscillator clock frequency in Hz if you want to get 40Mhz core clock in FEE mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CPU_INT_CLK_HZ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 31250u&amp;nbsp;&amp;nbsp; /* Value of the internal oscillator clock frequency in Hz&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define DEFAULT_SYSTEM_CLOCK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 32000000u /* Default System clock value */&lt;BR /&gt;&amp;nbsp; About the DEFAULT_SYSTEM_CLOCK&amp;nbsp; please note, if you BDIV is ICS-&amp;gt;C2 |= (uint8_t)(ICS_C2_BDIV(0x01));, then it should be 32Mhz/2=16Mhz.&lt;BR /&gt;&amp;nbsp; SystemCoreClockUpdate function, modify &lt;BR /&gt;&amp;nbsp; ICSOUTClock *= 1280u;&lt;BR /&gt;&amp;nbsp;to &lt;BR /&gt;&amp;nbsp; ICSOUTClock *= 1024u;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After you modify the header file, .s file and the clock system, then you can test it again.&lt;BR /&gt;If you still have question about the hardfault about uart, I suggest you comment all other code, just leave two UART.&lt;BR /&gt;You can just configure one uart1, then use it as the wake up source, then test it whether it still enter the hardfault or not?&lt;BR /&gt;When you disable the UART0, please clear the accoridng status at first, then disable it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you still have problems after all the above test, please kindly let me know.&lt;BR /&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 07:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEA-UART/m-p/857733#M51415</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-01-08T07:21:52Z</dc:date>
    </item>
  </channel>
</rss>