<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Programming K61using JTAG STAPL/SVF Format</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857568#M51389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Jochen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I double confirmed that&lt;/P&gt;&lt;P&gt;" NXP don't have tools for making that conversion. It is a bit more complicated than you realize. In order to program the flash, you need a flash algorithm. The way the debuggers/cyclone max handle it is they download a flash programming algorithm to the on-chip RAM, then pass it addresses and data for programming while controlling its execution via the debugger.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;So you need full run-control of the processor, not just scan chain capability, and the flash programming algorithm needs to be implemented."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2019 04:16:23 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2019-02-19T04:16:23Z</dc:date>
    <item>
      <title>Programming K61using JTAG STAPL/SVF Format</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857564#M51385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to program the K61 internal memory&lt;SPAN style="font-size: 11.0pt; color: black;"&gt; &lt;/SPAN&gt;without relying on other programmers like cyclone max, for automated programming during production tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an official NXP tool to convert the binary files I have to standard JTAG Files (STAPL/SVF)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They also come with 2 address offsets for the internal flash (BIOS/Application) which have to be considered when converting the binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 09:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857564#M51385</guid>
      <dc:creator>kaiser_jochen</dc:creator>
      <dc:date>2019-02-12T09:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: Programming K61using JTAG STAPL/SVF Format</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857565#M51386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, NXP does not provide&lt;SPAN class=""&gt; tool that convert binary files to STAPL or SVF.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I am really do not understand why customer need do like that, actually it is no meaning. Anyway, please make reference from below post on what we can do for this purpose:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2017/05/06/using-eclipse-to-program-binary-files-to-an-embedded-target/" title="https://mcuoneclipse.com/2017/05/06/using-eclipse-to-program-binary-files-to-an-embedded-target/"&gt;Using Eclipse to Program Binary Files to an Embedded Target | MCU on Eclipse&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 08:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857565#M51386</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-15T08:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: Programming K61using JTAG STAPL/SVF Format</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857566#M51387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the reason behind is that you don't have to use additional programmers for each product or device your are manufacturing/testing.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We use the official JTAG Controller from (&lt;A href="http://www.jtag.com)"&gt;www.jtag.com)&lt;/A&gt;. Even the NXP files were checked with their tools for their provided BSDL files. So why not supporting programming as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&amp;nbsp;&amp;nbsp; Device:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; K61 120MHz and 150MHz in 144BGA package&lt;BR /&gt;--&amp;nbsp;&amp;nbsp;&amp;nbsp; Package Type: K61_256BGA_17x17&lt;BR /&gt;--&lt;/P&gt;&lt;P&gt;--&amp;nbsp;&amp;nbsp; &amp;nbsp;This BSDL has been validated for syntax and semantics compliance to &lt;BR /&gt;--&amp;nbsp;&amp;nbsp; &amp;nbsp;IEEE 1149.1 using the JTAG Technologies CHKBSDL version 1.0.2.4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are so many different Microcontrollers/CPU/FPGA/CPLD etc. Imagine you use a test station where you have to put 15 USB Programmers inside and install 15 different Tools to program your stuff.&lt;/P&gt;&lt;P&gt;Some of them can't be automated due to missing CLI support, so you still have to click buttons.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Altera(Intel)/Microsemi or Xilinx/Lattice programming tools always provide functions to convert their files in the equivalent standardized SVF/JEDEC/STAPL format. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 09:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857566#M51387</guid>
      <dc:creator>kaiser_jochen</dc:creator>
      <dc:date>2019-02-15T09:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: Programming K61using JTAG STAPL/SVF Format</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857567#M51388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, understood. I will check internally and let you know if any feedback got.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 07:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857567#M51388</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-18T07:45:28Z</dc:date>
    </item>
    <item>
      <title>Re: Programming K61using JTAG STAPL/SVF Format</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857568#M51389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Jochen&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I double confirmed that&lt;/P&gt;&lt;P&gt;" NXP don't have tools for making that conversion. It is a bit more complicated than you realize. In order to program the flash, you need a flash algorithm. The way the debuggers/cyclone max handle it is they download a flash programming algorithm to the on-chip RAM, then pass it addresses and data for programming while controlling its execution via the debugger.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;So you need full run-control of the processor, not just scan chain capability, and the flash programming algorithm needs to be implemented."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 04:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-K61using-JTAG-STAPL-SVF-Format/m-p/857568#M51389</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2019-02-19T04:16:23Z</dc:date>
    </item>
  </channel>
</rss>