<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Starting with KL15 32-pin device</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232058#M5135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chiz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where did you find that example for the KL15?&amp;nbsp; I also use the KL25 development board and would like to use IAR.&amp;nbsp; Do you have one for the Keil compiler as well?&amp;nbsp; Would you mind sharing the examples?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Gil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jul 2014 22:05:31 GMT</pubDate>
    <dc:creator>gil1</dc:creator>
    <dc:date>2014-07-30T22:05:31Z</dc:date>
    <item>
      <title>Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232052#M5129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I designed a board with the MKL15Z128VFM4 which is essentially a 32-pin version of the KL15. I didn't want to use the uart pins seeing that I have a limited pin out. Therefore sysinit() and start() functions in the KL25FRDM family will have issues on my board because printf statements won't work.&lt;/P&gt;&lt;P&gt;Anyone know where to get small source code package with all the correct start, isr and low level routines needed to get a KL15 board going without needing all the KL25 FRDM board package?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Chiz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2013 23:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232052#M5129</guid>
      <dc:creator>Chiz</dc:creator>
      <dc:date>2013-09-13T23:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232053#M5130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Chiz&lt;/P&gt;&lt;P&gt;If you use our sample code, I think you might have to meet such a problem. Because sample code use UART to print information for demo. I suggest you use CodeWarrior to create a new project of KL15. If you want to use some basic module, you can use processor expert function in CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you. If&amp;nbsp; you meet question in your CodeWarrior develop process, please tell me. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Sep 2013 01:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232053#M5130</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-09-16T01:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232054#M5131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a way to work with the IAR tools. There is a "Getting Started" project which includes a minimal set of code necessary to start the chip. I found a similar set of start up code for the KL15 device family, and I'm working with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your suggestion.&lt;/P&gt;&lt;P&gt;Chiz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2013 12:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232054#M5131</guid>
      <dc:creator>Chiz</dc:creator>
      <dc:date>2013-09-17T12:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232055#M5132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;STRONG style="font-size: 12px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;A href="https://community.nxp.com/people/Paul.Tian"&gt;Paul.Tian&lt;/A&gt;&lt;/STRONG&gt;, &lt;/P&gt;&lt;P&gt;I have similar needs of &lt;EM&gt;Chiz Chikwendu&lt;/EM&gt; and I need to develop applications for KL14 with Codewarrior 10.4. I need to eliminate USB-UART but I would like to use previous projects developed for KL25. Could you suggest me the best way to proceede? Is it simpler to modify &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;sysinit() and start()&lt;/SPAN&gt; or I should desist and start from a new project? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2013 07:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232055#M5132</guid>
      <dc:creator>ulivinico</dc:creator>
      <dc:date>2013-09-20T07:24:39Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232056#M5133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same code should work for except the pin remapping. If you are concerned with printf then the printf will still work remapped to the board on your current board.&lt;/P&gt;&lt;P&gt;the startup codes and sysinit will remain same for most of the code except the USB clock Initialization part.&lt;/P&gt;&lt;P&gt;Don't see major changes in the code . In your existing project you can add the header and linker files of KL15 and according make the suitable changes.&lt;/P&gt;&lt;P&gt;While downloading in the download configuration choose the memory configuration file for KL15 and i think for the most part you will be fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any problems do let us know&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2013 10:11:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232056#M5133</guid>
      <dc:creator>deepakrana</dc:creator>
      <dc:date>2013-09-20T10:11:40Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232057#M5134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you. I've used the header file for MKL14 "MKL14Z4.h" generated by wizard. Concerning the linker, do you think it is possibile to use the one included in the &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;KL25 FRDM board package, i.e. "64KB_Pflash.ld" in the place of "128KB_Pflash.ld" (used by FREEDOM board)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Or should I use the MKL14Z64_flash.ld generated by the wizard?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2013 10:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232057#M5134</guid>
      <dc:creator>ulivinico</dc:creator>
      <dc:date>2013-10-02T10:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: Starting with KL15 32-pin device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232058#M5135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chiz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where did you find that example for the KL15?&amp;nbsp; I also use the KL25 development board and would like to use IAR.&amp;nbsp; Do you have one for the Keil compiler as well?&amp;nbsp; Would you mind sharing the examples?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Gil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2014 22:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Starting-with-KL15-32-pin-device/m-p/232058#M5135</guid>
      <dc:creator>gil1</dc:creator>
      <dc:date>2014-07-30T22:05:31Z</dc:date>
    </item>
  </channel>
</rss>