<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KE06Z Oscillator not working on custom board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853978#M51268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just assembled a custom board for a LQFP-44 package KE06Z chip. When I assembled everything, I put a scope on the oscillator to find that it's not oscillating. I used the FRDM-KE06Z as a reference design. This was a preliminary check and I have not actually tried flashing the chip yet. But my main question is if the oscillator should operate prior to flashing being that Xtal and EXTAL are the defaults for the pins&amp;nbsp;9 and 10 which using.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Where do the defaults in the datasheet actually come from? are they defauls in the SDK or are they defaults hardcoded in the chip from the factory?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 06 Jan 2019 06:58:49 GMT</pubDate>
    <dc:creator>stevenlutz</dc:creator>
    <dc:date>2019-01-06T06:58:49Z</dc:date>
    <item>
      <title>KE06Z Oscillator not working on custom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853978#M51268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just assembled a custom board for a LQFP-44 package KE06Z chip. When I assembled everything, I put a scope on the oscillator to find that it's not oscillating. I used the FRDM-KE06Z as a reference design. This was a preliminary check and I have not actually tried flashing the chip yet. But my main question is if the oscillator should operate prior to flashing being that Xtal and EXTAL are the defaults for the pins&amp;nbsp;9 and 10 which using.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Where do the defaults in the datasheet actually come from? are they defauls in the SDK or are they defaults hardcoded in the chip from the factory?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Jan 2019 06:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853978#M51268</guid>
      <dc:creator>stevenlutz</dc:creator>
      <dc:date>2019-01-06T06:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: KE06Z Oscillator not working on custom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853979#M51269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The crystal oscillator will only start when you load code to program it (in OSC0_CR). It will not oscillate by default, even though the pins default to that mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;SPAN&gt;Complete Solutions and technical support for professional Kinetis developments: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 04:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853979#M51269</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2019-01-07T04:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: KE06Z Oscillator not working on custom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853980#M51270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Mark is correct.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If you want to observe the oscillating, please try to flash corresponding program first.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Robin&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 08:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06Z-Oscillator-not-working-on-custom-board/m-p/853980#M51270</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-01-08T08:55:08Z</dc:date>
    </item>
  </channel>
</rss>