<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUnable to program KL03 below 2.7VDC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851892#M51203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In conjunction with Kinetis Design Studio, I am using a Multilink Universal device to program NXP MKL03Z32CAFR MCUs that are powered off of a 2.1 V supply in my design. I am getting a P&amp;amp;E Connection Assistant message when my MCU is powered from 2.1 V, and cannot program the MCU. When the MCU is powered at 3 V, I do not get the error and can successfully program the MCU.&lt;/P&gt;&lt;P&gt;The only way I am able to program my MCU at 2.1V is to first use the Kinetis Recovery Tool utility to halt the processor.&lt;/P&gt;&lt;P&gt;Are there other flash algorithms that will automatically halt the processor immediately upon startup? Any suggestions would be helpful.&lt;/P&gt;&lt;P&gt;-Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jan 2019 20:57:41 GMT</pubDate>
    <dc:creator>aboss</dc:creator>
    <dc:date>2019-01-03T20:57:41Z</dc:date>
    <item>
      <title>Unable to program KL03 below 2.7VDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851892#M51203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In conjunction with Kinetis Design Studio, I am using a Multilink Universal device to program NXP MKL03Z32CAFR MCUs that are powered off of a 2.1 V supply in my design. I am getting a P&amp;amp;E Connection Assistant message when my MCU is powered from 2.1 V, and cannot program the MCU. When the MCU is powered at 3 V, I do not get the error and can successfully program the MCU.&lt;/P&gt;&lt;P&gt;The only way I am able to program my MCU at 2.1V is to first use the Kinetis Recovery Tool utility to halt the processor.&lt;/P&gt;&lt;P&gt;Are there other flash algorithms that will automatically halt the processor immediately upon startup? Any suggestions would be helpful.&lt;/P&gt;&lt;P&gt;-Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 20:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851892#M51203</guid>
      <dc:creator>aboss</dc:creator>
      <dc:date>2019-01-03T20:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program KL03 below 2.7VDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851893#M51204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew,&lt;/P&gt;&lt;P&gt;There isn't other flash algorithm. You have to find out why the mcu brick. KL03 can be programed at 1.8V. I guess below 2.7V the MCU is affected by other device and circuits on the board, or by improper setting. I attached some links you can refer to.&amp;nbsp; They are for KL25. But KL03 is also fit for it.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/324790"&gt;kinetis KL2x programming voltage @ 1.8V&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/304539"&gt;https://community.nxp.com/message/304539&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 09:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851893#M51204</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-01-04T09:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program KL03 below 2.7VDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851894#M51205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the information Jing. I have made modifications to my board by removing all of the non-essential components required for programming. All that remains is the MCU, 10k pull up resistor on the reset pin and a 0.1 uF decoupling capacitor for the MCU power pin, along with the traces leading to the SWD programming connector, i.e. only parts related to the SWD interface. I am still unable to program the MCU at supply voltages below 2.7 V, unless I first halt the processor using the Kinetis Recovery Tool. I only have success without using the Kinetis Recovery Tool&amp;nbsp;with voltages above 2.7 V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU I am working with on my board was ordered from our CM back in June of 2018. If I try a simple breadboard setup with an MCU that was ordered over two years ago, I do not have an issue programming at voltages below 2.7 V. Please note that the breadboard setup and my PCB setup are similar in nature now that I have removed all non-SWD related components.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am suspecting the core is going into an infinite reset once it detects the supply is below 2.7 V based on Table 7 of section 2.2.2 of the KL03 Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Andrew&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 15:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851894#M51205</guid>
      <dc:creator>aboss</dc:creator>
      <dc:date>2019-01-04T15:04:42Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to program KL03 below 2.7VDC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851895#M51206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew,&lt;/P&gt;&lt;P&gt;Please check PMC_LVDSC1 register. By default, LVDRE=1 and LVDV=0. This mean LVD reset enable and low trip point selected. The V LVDL is around 1.60v(datasheet Table 6). If you change this setting to LVDH, reset will occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 08:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Unable-to-program-KL03-below-2-7VDC/m-p/851895#M51206</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-01-07T08:45:28Z</dc:date>
    </item>
  </channel>
</rss>