<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: A complete tutorial of editing linker file in MCUExpresso IDE in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-complete-tutorial-of-editing-linker-file-in-MCUExpresso-IDE/m-p/851209#M51167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick Ng,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; About the MCUXpresso IDE linker file modification tutorial, please refer to this document:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-335283"&gt;Relocating Code and Data Using the MCUXpresso IDE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It is very clear to help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jan 2019 08:48:56 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2019-01-23T08:48:56Z</dc:date>
    <item>
      <title>A complete tutorial of editing linker file in MCUExpresso IDE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-complete-tutorial-of-editing-linker-file-in-MCUExpresso-IDE/m-p/851208#M51166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently trying to modify a linker file&amp;nbsp;for a &amp;nbsp;k66 MCU with 2 MB flash and 192K + 64K RAM.&lt;/P&gt;&lt;P&gt;My target is to place a small ram&amp;nbsp;region ~100 Bytes of data at the end of that upper ram (192K one) , so that I can&amp;nbsp; share the data between the bootloader and the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any tutorial and example to show how to do so?&lt;/P&gt;&lt;P&gt;I see there is config setting at the project property of the MCUExpresso&amp;nbsp; &amp;nbsp;project, which I can use to add/modify the ram layout. But I am not sure how use it correctly...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63995i772DD8E9D8A1F21D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 04:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-complete-tutorial-of-editing-linker-file-in-MCUExpresso-IDE/m-p/851208#M51166</guid>
      <dc:creator>nick_ng</dc:creator>
      <dc:date>2019-01-22T04:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: A complete tutorial of editing linker file in MCUExpresso IDE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-complete-tutorial-of-editing-linker-file-in-MCUExpresso-IDE/m-p/851209#M51167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nick Ng,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; About the MCUXpresso IDE linker file modification tutorial, please refer to this document:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-335283"&gt;Relocating Code and Data Using the MCUXpresso IDE&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; It is very clear to help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 08:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-complete-tutorial-of-editing-linker-file-in-MCUExpresso-IDE/m-p/851209#M51167</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-01-23T08:48:56Z</dc:date>
    </item>
  </channel>
</rss>