<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: How to load usb stack to DDR memory</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231953#M5115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I know, K70 has two PLLs , PLL1 is dedicated for DDR , and PLL0's output can be used for USB module, I am not sure how you configure them, but in my opinion , PLL0 should output 48MHz for USB application, PLL1 may output as high as possible to meet the DDR2 spec. so please check the PLL initialization first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Jun 2013 07:26:43 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2013-06-21T07:26:43Z</dc:date>
    <item>
      <title>How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231950#M5112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how can i load Usb Stack program to K70 controller DDR memory.&lt;/P&gt;&lt;P&gt;I want to add a debug configuration to run USb stack from DDR memory&lt;/P&gt;&lt;P&gt;Plz can any one help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 04:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231950#M5112</guid>
      <dc:creator>abhilash</dc:creator>
      <dc:date>2013-06-21T04:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231951#M5113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The released demo just support flash and RAM target, but I think you may use the RAM target&amp;nbsp; as a starting point. &lt;/P&gt;&lt;P&gt;The main differences with a standard “RAM target” are :&lt;/P&gt;&lt;P&gt;− Appropriate linker file&lt;/P&gt;&lt;P&gt;− Macro set-up file that initializes the DRAM chip before the J-link starts download.&lt;/P&gt;&lt;P&gt;they can be both referred to 128MB_DDR2.icf from &lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;KINETIS_120MHZ_SC, and K70_MT47H64M16HR-3.mac as well.&lt;/P&gt;&lt;P&gt;Please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119511iC5DA0A251E04383C/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.PNG" alt="1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119512i9EE08A01B6357B94/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.PNG" alt="2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 05:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231951#M5113</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-06-21T05:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231952#M5114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the information&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;P&gt;I followed your instruction and used linker files from &lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;KINETIS_120MHZ_SC for DDR(128MB_ddr.lcf) and ram(MK70FN1M0_ram.lcf). Also we are using initialization file for the DDR (init_twr_k70_ddr2.tcl). But when i loaded and started running the program it exits when&amp;nbsp; TestApp_Init(); function is called .The program runs fine when run from flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;{ I am running USB stack 4.1.1&amp;nbsp; CDC sample program in High speed config using code warrior IDE10.2 and OSJTAG downloader }&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 07:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231952#M5114</guid>
      <dc:creator>abhilash</dc:creator>
      <dc:date>2013-06-21T07:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231953#M5115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I know, K70 has two PLLs , PLL1 is dedicated for DDR , and PLL0's output can be used for USB module, I am not sure how you configure them, but in my opinion , PLL0 should output 48MHz for USB application, PLL1 may output as high as possible to meet the DDR2 spec. so please check the PLL initialization first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 07:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231953#M5115</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-06-21T07:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231954#M5116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello kan,&lt;/P&gt;&lt;P&gt;inside the init file pll1 is configured and it is used for ddr configuration. when using DDR memory&amp;nbsp; Sysinit function is not working.For now i have it disabled. Now my doubt is on the linker file . Is there any specific linker file that can be used with USB stack&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;Abhi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Jun 2013 11:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231954#M5116</guid>
      <dc:creator>abhilash</dc:creator>
      <dc:date>2013-06-21T11:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231955#M5117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abhi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late response!! I had some issue with my IAR license until I re-installed it. I have implemented the CDC demo running in DDR based on TWR-K70, but It is not only the link file, but also the&amp;nbsp; PLL init function called in the usb stack should be modified to make the usb stack run in DDR. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First , I recommend you start with a SRAM target configuration, &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119513i8A7E17F70837D6FC/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;second, just as mentioned before, use mac file to initialize the PLL0 and PLL1 as well as the DDR controller before the IDE load the image.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119514iF404F6F56070DD92/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and choose verify download if you like&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119515i6679AEADC6265543/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then, you may change the sram link file as the following:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119516iAC51E64AB7FA8041/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;you may find the RAM section are in DDR now, but please note don't set 0x08000000 to 0x10000000 as the range, this configuration are used by KINETIS120MHZ_SC, but as the USB stack uses DMA to transmit or receive data, you have to put the section in a location that allow access from both core and eDMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and set the vector table in SRAM.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119517i0579DB7D20EF8F8B/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As PLL0 and PLL1 have been initialized in the mac file, there is no need to do it in SYS_Init(), add some code from line 884 in main_kinetis,c&lt;/P&gt;&lt;P&gt;#ifdef SDRAM &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialize clocks to match values from init script */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mcg_clk_hz = 120000000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pll_1_clk_khz = 150000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pll_0_clk_khz = mcg_clk_hz / 1000;&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;P&gt;#define ASYNCH_MODE&amp;nbsp;&amp;nbsp;&amp;nbsp; /* PLL1 is source for MCGCLKOUT and DDR controller */&lt;/P&gt;&lt;P&gt;#define SDRAM&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;and #endif at line 924.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Define SDRAM in "derivative,h "&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#define SDRAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that, run the application , you will see the following view:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119518i32EEED275D03D3DE/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and found the cdc device in the device manager:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119519iC90FB9390EDD2EB3/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice weekend!!&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2013 09:39:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231955#M5117</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2013-06-28T09:39:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to load usb stack to DDR memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231956#M5118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi @abhilash&amp;nbsp; did you get the USB stack to work fine from DDR? Would you be kind enough to attach it here ? We are facing the very same issue. It runs fine in Flash, but the DDR build just won't work. We've tried everything from changes in linker file to tcl script to watchdog. Your project will really help us. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 05:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-load-usb-stack-to-DDR-memory/m-p/231956#M5118</guid>
      <dc:creator>reubennoronha</dc:creator>
      <dc:date>2015-08-11T05:06:56Z</dc:date>
    </item>
  </channel>
</rss>