<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: mpc5744 Adc sampling inaccurate</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mpc5744-Adc-sampling-inaccurate/m-p/849974#M51131</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Do you use our EVB for these tests or its your own custom board?&lt;/P&gt;&lt;P&gt;Do you calibrate ADCs before conversion?&lt;/P&gt;&lt;P&gt;Did you tried to measure it on different pins for ADC1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 May 2019 10:29:43 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2019-05-14T10:29:43Z</dc:date>
    <item>
      <title>mpc5744 Adc sampling inaccurate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mpc5744-Adc-sampling-inaccurate/m-p/849973#M51130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPC5744P chip ADC sampling, the reference voltage is 5V ,ADC0 and ADC1 sampling port peripheral reference voltage circuits are the same. The software is configured with ADC0 port 0 channel, ADC1 port 0 channel sampling at the same time, the external input analog voltage has 0 ~ 5 V change; Phenomenon: ADC0 port 0 channel sampling is normal, external voltage 2.5 V shows AD value 2045; When the external voltage of the ADC1 port 1 channel is 2.5V, the AD value 1750A DC0 changes linearly with the external voltage analog signal, and the ADC1 changes linearly with the external voltage analog signal (0 v corresponding to AD value 0 V to 5 v to AD value 4095, intermediate nonlinearity).&lt;/P&gt;&lt;P&gt;May I ask which points may have caused this phenomenon to occur?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Dec 2018 15:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mpc5744-Adc-sampling-inaccurate/m-p/849973#M51130</guid>
      <dc:creator>chenbg188175751</dc:creator>
      <dc:date>2018-12-09T15:16:13Z</dc:date>
    </item>
    <item>
      <title>Re: mpc5744 Adc sampling inaccurate</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mpc5744-Adc-sampling-inaccurate/m-p/849974#M51131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Do you use our EVB for these tests or its your own custom board?&lt;/P&gt;&lt;P&gt;Do you calibrate ADCs before conversion?&lt;/P&gt;&lt;P&gt;Did you tried to measure it on different pins for ADC1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 10:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mpc5744-Adc-sampling-inaccurate/m-p/849974#M51131</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2019-05-14T10:29:43Z</dc:date>
    </item>
  </channel>
</rss>