<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: BOOTCFG pin active high or low</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849499#M51106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you! Apparently putting a high value at the pin will result in a 1 at the register. I missed that point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2018 14:59:01 GMT</pubDate>
    <dc:creator>wilco_work</dc:creator>
    <dc:date>2018-09-27T14:59:01Z</dc:date>
    <item>
      <title>BOOTCFG pin active high or low</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849497#M51104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the K82FN256 and want to use the BOOTCFG0 pin for booting. Is this BOOTCFG0 active HIGH or active LOW (asserted by logic 1 or 0)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kin regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 10:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849497#M51104</guid>
      <dc:creator>wilco_work</dc:creator>
      <dc:date>2018-09-20T10:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: BOOTCFG pin active high or low</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849498#M51105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on the following table of the reference manual.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69398iA7C3A274DFA71B66/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We can know that the pin is active high, asserted by logic 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 17:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849498#M51105</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-21T17:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: BOOTCFG pin active high or low</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849499#M51106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you! Apparently putting a high value at the pin will result in a 1 at the register. I missed that point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 14:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BOOTCFG-pin-active-high-or-low/m-p/849499#M51106</guid>
      <dc:creator>wilco_work</dc:creator>
      <dc:date>2018-09-27T14:59:01Z</dc:date>
    </item>
  </channel>
</rss>