<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKW41Z setting DC-DC voltage</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849228#M51088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application where&amp;nbsp;an ftdi chip for USB is powered by the on board dc to dc converter in the KW41Z (specifically I am using a rigado Bluetooth module). I was able to set the voltage when I am running FreeRTOS using the DCDC.h from the sdk framework, but my current applications cannot use an OS so I need to be able to set up the output of the dc to dc converter using the fsl_dcdc driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having no luck with this. Does anyone know to use this driver or have any example code that uses it? Is it possible to just write directly to the register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#KW41Z #DCDC #fsl_dcdc #rigado&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jul 2018 13:07:15 GMT</pubDate>
    <dc:creator>mitchenerjosh</dc:creator>
    <dc:date>2018-07-04T13:07:15Z</dc:date>
    <item>
      <title>KW41Z setting DC-DC voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849228#M51088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application where&amp;nbsp;an ftdi chip for USB is powered by the on board dc to dc converter in the KW41Z (specifically I am using a rigado Bluetooth module). I was able to set the voltage when I am running FreeRTOS using the DCDC.h from the sdk framework, but my current applications cannot use an OS so I need to be able to set up the output of the dc to dc converter using the fsl_dcdc driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having no luck with this. Does anyone know to use this driver or have any example code that uses it? Is it possible to just write directly to the register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#KW41Z #DCDC #fsl_dcdc #rigado&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 13:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849228#M51088</guid>
      <dc:creator>mitchenerjosh</dc:creator>
      <dc:date>2018-07-04T13:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z setting DC-DC voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849229#M51089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/mitchenerjosh"&gt;mitchenerjosh&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have an example of how to use the fsl_dcdc driver off hand, but we do discuss how to adjust the target voltage via direct register writes in this application note:&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5025.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN5025.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Specifically this subject is covered in section 4.2.1 Target Voltage Adjustment.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you have other questions or concerns.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chris&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 16:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849229#M51089</guid>
      <dc:creator>chris_brown</dc:creator>
      <dc:date>2018-07-05T16:12:21Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z setting DC-DC voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849230#M51090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After following the flowchart I was able to set the voltage.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jul 2018 20:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW41Z-setting-DC-DC-voltage/m-p/849230#M51090</guid>
      <dc:creator>mitchenerjosh</dc:creator>
      <dc:date>2018-07-09T20:45:37Z</dc:date>
    </item>
  </channel>
</rss>