<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックS9KEAZN64 doesn't run code from flash after power reset</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848573#M51052</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I have make a custome board with S9KEAZN64 MCU and got next trouble. I am using segger j-link edu for programming and debug. I wrote software led blink for test and start debug it. All work correcty but when i stop debug and reset power it doesn't start again. Code running from flash and i checked flash memory via segger. Binary are there. I tried to make reset pin low and high back but it doesn't help. But it is possible to start it via J-Link tool(button named start mcu or similar). What can be wrong? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Dec 2018 22:38:34 GMT</pubDate>
    <dc:creator>vitaliharudka</dc:creator>
    <dc:date>2018-12-07T22:38:34Z</dc:date>
    <item>
      <title>S9KEAZN64 doesn't run code from flash after power reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848573#M51052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I have make a custome board with S9KEAZN64 MCU and got next trouble. I am using segger j-link edu for programming and debug. I wrote software led blink for test and start debug it. All work correcty but when i stop debug and reset power it doesn't start again. Code running from flash and i checked flash memory via segger. Binary are there. I tried to make reset pin low and high back but it doesn't help. But it is possible to start it via J-Link tool(button named start mcu or similar). What can be wrong? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 22:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848573#M51052</guid>
      <dc:creator>vitaliharudka</dc:creator>
      <dc:date>2018-12-07T22:38:34Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN64 doesn't run code from flash after power reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848574#M51053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi VITALI,&lt;/P&gt;&lt;P&gt;S9KEA boot up sequence is simple and directly. When the processor exits reset, it performs the following:&lt;/P&gt;&lt;P&gt;• Reads the start SP (SP_main) from vector-table offset 0&lt;BR /&gt;• Reads the start program counter (PC) from vector-table offset 4&lt;BR /&gt;• The Link Register (LR) is set to 0xFFFF_FFFF.&lt;/P&gt;&lt;P&gt;You can see these words in reference manual 6.2.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe you can check&amp;nbsp;4 point:&lt;/P&gt;&lt;P&gt;1. Is there a 4.7uF or above capacitor on VDD. Without this cap, latch-up may happen.&lt;/P&gt;&lt;P&gt;2. May it caused by improper watchdog setting?&lt;/P&gt;&lt;P&gt;3. Is hardware design or welding ok?&lt;/P&gt;&lt;P&gt;4. Is the project setting well? Can other demo code run correctly.&lt;/P&gt;&lt;P&gt;Please try this driver library:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FRDM-KEXX-Driver-Library-Package&amp;amp;location=null"&gt;https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FRDM-KEXX-Driver-Library-Package&amp;amp;location=null&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is for KExx, but it also can run on KEA. They are all same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please&amp;nbsp;also try&amp;nbsp;device demos in &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/nxp-freedom-development-platform-for-ultra-reliable-kinetis-ea-series-mcus:FRDM-KEAZ128?tab=Design_Tools_Tab"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/nxp-freedom-development-platform-for-ultra-reliable-kinetis-ea-series-mcus:FRDM-KEAZ128?tab=Design_Tools_Tab&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2018 07:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848574#M51053</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-12-10T07:36:33Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN64 doesn't run code from flash after power reset</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848575#M51054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It was required to off NMI. While debugging it off automatically but after power reset it's turn on and mcu stuck in interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 10:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN64-doesn-t-run-code-from-flash-after-power-reset/m-p/848575#M51054</guid>
      <dc:creator>vitaliharudka</dc:creator>
      <dc:date>2019-03-20T10:53:54Z</dc:date>
    </item>
  </channel>
</rss>