<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is PN5180 VHDF output sufficient for K81 LLWU input?   in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847884#M51038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I see that the K8x has a comparator peripheral, so no additional external hardware may be required.&amp;nbsp; I guess the question then becomes:&amp;nbsp; Can the K8x's onboard comparator be used as a wakeup source?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Dec 2018 19:05:32 GMT</pubDate>
    <dc:creator>deniscollis</dc:creator>
    <dc:date>2018-12-07T19:05:32Z</dc:date>
    <item>
      <title>Is PN5180 VHDF output sufficient for K81 LLWU input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847883#M51037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the PN5180's Zero Power Wakeup feature to interrupt/wake-up the K8x.&amp;nbsp; The theory appears to be that energy from, say, a smart phone NFC is received by the PN5180's antenna and sent directly out the VDHF pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is whether the PN5180's VDHF output can be directly connected to the K8x's LLWU input, or if the VHDF output signal must first be conditioned by some device, like a comparator with push-pull output, to provide sufficient power to trip the LLWU?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For simplicity of design I would favor the direct option, if it works!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 18:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847883#M51037</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-12-07T18:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: Is PN5180 VHDF output sufficient for K81 LLWU input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847884#M51038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I see that the K8x has a comparator peripheral, so no additional external hardware may be required.&amp;nbsp; I guess the question then becomes:&amp;nbsp; Can the K8x's onboard comparator be used as a wakeup source?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 19:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847884#M51038</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-12-07T19:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: Is PN5180 VHDF output sufficient for K81 LLWU input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847885#M51039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, K8x comparator module can work as a wakeup source.&lt;/P&gt;&lt;P&gt;Please check below comparator working status during each low power mode:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69154iE7CC3D9D0333CDC7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69326i411CC8D4DA4540F7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69230i5B9BDF7AD3DB4541/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CMP modules are also wakeup source of LLWU:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69272i00C5673F47791A30/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 06:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847885#M51039</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-12-12T06:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Is PN5180 VHDF output sufficient for K81 LLWU input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847886#M51040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mike.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is helpful info, but I&amp;nbsp;just need to add:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is just one VDHF output from the PN5180 for the CMP-INP(PSEL[2:0]).&amp;nbsp;&amp;nbsp;I must therefore use the DAC to provide the reference voltage to CMP-INM(MSEL[2:0].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know if there is any example code specifically for the Zero Power Wakeup on the&amp;nbsp; PN5180/K81 coupled devices?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;Denis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Dec 2018 01:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847886#M51040</guid>
      <dc:creator>deniscollis</dc:creator>
      <dc:date>2018-12-13T01:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: Is PN5180 VHDF output sufficient for K81 LLWU input?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847887#M51041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From PN5180 aspect, there doesn't need software to enable Zero Power Wakeup feature.&lt;/P&gt;&lt;P&gt;No configuration of registers is required to use this functionality.&lt;/P&gt;&lt;P&gt;The VDHF pin need connect&amp;nbsp; with 470nF capacitor to GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From K81 aspect, customer can refer &lt;A href="https://mcuxpresso.nxp.com/en/dashboard"&gt;MCUXpresso SDK&lt;/A&gt; [cmp] software example for K81 CMP module application.&lt;/P&gt;&lt;P&gt;Customer also can refer [power_manager] demo about K81 how to enter low power mode and how to wake up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2018 02:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-PN5180-VHDF-output-sufficient-for-K81-LLWU-input/m-p/847887#M51041</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-12-14T02:51:56Z</dc:date>
    </item>
  </channel>
</rss>