<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Quadrature Decoder not counting correctly on FRDM-K66F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847342#M51003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Status Update.&amp;nbsp; If I connect a signal generator signal 0 to 3.3V square wave running at 1000Hz on to the Freedom board Phase A pin with Phase B pin pulled up to 3.3v or down to GND with a resistor, and switch FTM Quadrature Decoder Mode from&amp;nbsp;Phase A and Phase B encoding mode TO&amp;nbsp;&amp;nbsp;Count and Direction encoding mode,&amp;nbsp; &amp;nbsp;I get a count of +250 or -250 depending on the logic value on Phase B pin.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2018 14:16:55 GMT</pubDate>
    <dc:creator>jeffsylvester</dc:creator>
    <dc:date>2018-10-02T14:16:55Z</dc:date>
    <item>
      <title>Quadrature Decoder not counting correctly on FRDM-K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847339#M51000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have FRDM-K66F and using a CUI inc Encoder AMT213B-V that has 1024 PPR (pulse per revolution) and I have it connected to FTM1 on FRDM board.&amp;nbsp; (because I also need CAN0 that shares I/O pins with FTM2 on PTB18,PTB19.&amp;nbsp; &amp;nbsp;So I used MCUExpresso Config Tool to set up the FTM1 pins, and registers,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I run example code from Quadrature Encode/Decode example in SDK for FRDM-K66F that uses PIT timer to do a once per second read of the count register of FTM.&amp;nbsp; &amp;nbsp; This example manually does some setting up of FTM so I comment this out and use the BOARD_InitPeripherals(), BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole()&lt;/P&gt;&lt;P&gt;to set up all the registers at boot time.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have viewed the encoder output and the signals look just fine with A and B signals 90Degrees out of phase with each other and signal is solid 3.3V&amp;nbsp; ( encoder outputs 5v signal that goes through a 5v to 3.3v voltage translator.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;when I spin the encoder one full revolution,&amp;nbsp; i should get 4096 Edges counted.&amp;nbsp; (for both rising and falling edges on both A and B as per manual page 1254 of K66 Sub Family Reference Manual Rev&amp;nbsp; 2 May 2015&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I spin the encoder at a slow rate about one revolution per 1/2 second.&amp;nbsp; &amp;nbsp;and I Measure around 3800 PPR in both + and - directions.&amp;nbsp; &amp;nbsp; So this tells me one of three possibilities.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) The encoder puts out less PPR than stated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) the Quadrature Decoder is not working / counting properly&lt;/P&gt;&lt;P&gt;3) The settings for FTM are not correct causing #2 above&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See attachment.&amp;nbsp; &amp;nbsp; Clock settings are Core clock 120MHz, System clock 120MHz, Bus Clock 60MHz, OSCERCLK 12MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried Input filter settings of 1 to 12 on both channels A and B and the number does not seem to change the 3800PPR I am seeing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have and suggestions on how to fix?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Sep 2018 14:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847339#M51000</guid>
      <dc:creator>jeffsylvester</dc:creator>
      <dc:date>2018-09-19T14:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Decoder not counting correctly on FRDM-K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847340#M51001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the decoder for FRDM-K66F, I think the example code is fine, the encoder sensor hardware is fine, the difference between the expected counting and the actual counting is the position error you spins the rotor manually.&lt;/P&gt;&lt;P&gt;I suggest you do not read the FTM counter in PIT ISR. After You start counting, you can spin the rotor multiple revolutions for example 10 revolutions, then in the debugger, break the code and read the FTM counter, in this way, the accumulative error can be reduced by average.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 06:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847340#M51001</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-09-20T06:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Decoder not counting correctly on FRDM-K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847341#M51002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have got this response from filing a tech support ticket:&amp;nbsp; &amp;nbsp;It has some good advise on how to debug, and other ways to try to do comparison testing.&amp;nbsp; &amp;nbsp; so I will post this here for others to read.&amp;nbsp; however it still misses the main point that I already know that the encoder outputs 1024 PPR pulse per revolution.&amp;nbsp; &amp;nbsp;I suspect that some how in firmware the registers are not set up or have some kind of conflict?&amp;nbsp;&amp;nbsp;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;I have attached a COPAL RE30E1024-213 -1 Encoder to FRDM-K66F devboard at FTM1 pins PTA8 and PTA9. I get very stable Encoder pulse signal.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE border="0" cellpadding="5" cellspacing="5" height="400" style="color: #000000; background-color: transparent; font-size: 16px;" width="600"&gt;&lt;TBODY&gt;&lt;TR valign="top"&gt;&lt;TD style="color: #000000; background-color: #ffffff; font-size: 12pt;"&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;Dear Jeff Sylvester,&amp;nbsp;&lt;/SPAN&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR valign="top"&gt;&lt;TD style="color: #000000; background-color: #ffffff; font-size: 12pt;"&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;Regarding your question, it is difficult to make a conclusion that the code or Decoder hardware has issue. The key is that you have to know how many pulses has been generated by the Encoder after you spin the rotor manually.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: small;"&gt;In order to know pusle number the encoder generates, I think you can use capture function of FTM, in detail, you can connect one Encoder signal(PhaseA or PhaseB, not both) to FTM2_CHx, configure the channel of FTM2 in capture mode to generate capture interrupt with rising edge , in the capture ISR, you can increase a variable by 1, in this way, you can know how many pulses has been generated, then you can compare the quadrature counter and the pulse variable and check if they match or not.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: small;"&gt;Another method is that you connect the PhaseA for example to LPTMR_ALT1(PTC5), then configure theLPTMR to count the pulse rising edge, then compare the LPTMR counter and the quadrature counter.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: small;"&gt;Hope it can help you&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;To update this case, please reply to this email.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;Thank you for your interest in NXP Semiconductor products and&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;for the opportunity to serve you.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;Best regards,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;X.j.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;Technical Support&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: arial; font-size: small;"&gt;NXP Semiconductor&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2018 20:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847341#M51002</guid>
      <dc:creator>jeffsylvester</dc:creator>
      <dc:date>2018-09-27T20:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Decoder not counting correctly on FRDM-K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847342#M51003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Status Update.&amp;nbsp; If I connect a signal generator signal 0 to 3.3V square wave running at 1000Hz on to the Freedom board Phase A pin with Phase B pin pulled up to 3.3v or down to GND with a resistor, and switch FTM Quadrature Decoder Mode from&amp;nbsp;Phase A and Phase B encoding mode TO&amp;nbsp;&amp;nbsp;Count and Direction encoding mode,&amp;nbsp; &amp;nbsp;I get a count of +250 or -250 depending on the logic value on Phase B pin.&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 14:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847342#M51003</guid>
      <dc:creator>jeffsylvester</dc:creator>
      <dc:date>2018-10-02T14:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: Quadrature Decoder not counting correctly on FRDM-K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847343#M51004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wrote a program to output encoder signals on PTD12 and PTD13 on the FREEDOM board to eliminate any possibility of bad voltage or noise signals from a physical encoder,&amp;nbsp; i input these into FTM1 phase A and B,&amp;nbsp; and run program.&amp;nbsp; Turns OUT that the SemiHosting Debugging is causing the errors.&amp;nbsp; it completely stops the processor and interrupts during "Console Talking" and is the reason for the errors.&amp;nbsp; If program is run without debug console it works as intended.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 21:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Quadrature-Decoder-not-counting-correctly-on-FRDM-K66F/m-p/847343#M51004</guid>
      <dc:creator>jeffsylvester</dc:creator>
      <dc:date>2018-10-10T21:22:02Z</dc:date>
    </item>
  </channel>
</rss>